STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can we take TIMER2, Channel3 for External clock mode1 for frequency counting upto 5-10 MHZ? Board: STM32F401RE [Nucleo Board], PIN: PB_10 [Timer 2, channel3]

Can we take TIMER2, Channel3 for External clock mode1 for frequency counting upto 5-10 MHZ? Board: STM32F401RE [Nucleo Board], PIN: PB_10 [Timer 2, channel3].In case, yes.. Can anybody provide me refrence or sample code?

SRai.17 by Associate II
  • 1682 Views
  • 4 replies
  • 0 kudos

Stm32l011k4 and Adafruit Sharp memory display breakout

Hello, I am trying to use the STM32l011k4 with the Sharp memory display breakout from Adafruit. I succeeded in clearing the screen but I can't display a pixel on the screen. I always have the same display, probably what the buffer contains. I don't k...

Jean1 by Associate
  • 800 Views
  • 0 replies
  • 0 kudos

STM32F303 OPAMP Timer controlled Multiplexer mode

I'd like to amplify two signals connected to non-inverting input of OPAMP and control which one is currently amplified by TIM1, Channel 6. This technique is described in RM0316 document, chapter 18.3.6 Timer controlled Multiplexer mode.I've set TIM1,...

0690X000006BwyUQAS.png

STemWin

I have managed to get STemWin showing the "Hello World" message on the STM32F779I-EVAL board using CubeMX.The project has FreeRTOS enabled.Maybe it's me not understanding STemWin... but it seems after the screen refresh during the initialization, STe...

TDahl by Associate II
  • 831 Views
  • 0 replies
  • 0 kudos

Is that possible to use SWO without Debugger?

Hi,​My target is STM32L151 (Cortex M3). ​I would like to print data through SWO without a debugger connected to SWD . Is it possible? If it is, should I configure something in the STM32? Thank you for any help!​

Yevpator by Associate III
  • 2617 Views
  • 5 replies
  • 0 kudos