STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32h7xx_hal_usart.h include guard is incorrect.

There is a "2" missing in the define at the beginning of the stm32h7xx_hal_usart.h file. Can somebody fix it for the next release? - if there is one./* Define to prevent recursive inclusion -------------------------------------*/#ifndef __STM32H7xx_H...

[stm32f407] Resets RTC and backup registers after power off

Good day. A strange problem. After turning off the power, the backup registers and the real time clock are reset.Could it be that I messed up at initialization, or something that I missed?void RTC_init( void ) { RTC_InitTypeDef rtc; RTC_InitTyp...

0690X000006BzQVQA0.jpg
EKoro by Associate
  • 1485 Views
  • 4 replies
  • 0 kudos

STM32 interrupt priority

HiI want to set interrupt priority for TIM3. So I made configuration in NVIC register.But I met some question.the base adress of NVIC in STM32F10xxx Cortex-M3 programming manual is 0XE000E100 ,but in another book STM32F10xxx Cortex-M3 programming man...

0690X000006BzXlQAK.png 0690X000006BzY0QAK.png
kang by Associate
  • 2572 Views
  • 2 replies
  • 0 kudos

How to use CMake compile STM32CubeL4 Firmware Package?

I saw there is CMakeLists.txt in the folder, should be able to use CMake. The problem is I am choose different MinGW makefile format, never success. The reason for me to use CMake is to compile GoogleTest, I won't compile in the atolic TrueStudio. My...

Plug and play evalboard for Bluetooth audio

Hey guys i am searching an easy plug and play bluetooth audio solution possibly build on an stm32 nucleo that would perfectly also have a 5 - 10W amp included. Is there also a solution with audio weaver where i can program easily filters for left and...

What is the chip of the STM32 control board?

Hello. I am analyzing to acquire the EVALKITST8500-1, however I had some doubts regarding some aspects of the board. The STM32 board control board that comes in the kit anyone what model of the STM 32 chip is it? Or can you put any chip on the contro...

??sil by Associate
  • 671 Views
  • 1 replies
  • 0 kudos