cancel
Showing results for 
Search instead for 
Did you mean: 

Control 2 MIPI-DSI AMOLED screens with STM32F769I-DISCO

Carlos Camacho
Associate
Posted on May 29, 2018 at 13:41

Hello,

I'll like to know if it's possible to drive two MIPI-DSI screens (

LS029B3SX02 and

passing the same signal to both displays), with a STM32F769I-DISCO eval board.

The thing is that I need to be able to add an HDMI and a CVBS video input to pass it to the screens.

Thanks,

Carlos.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
T J
Lead
Posted on May 29, 2018 at 15:01

To see the exact same image on both displays, maybe, depends on the length of the two display cables.

To see different images ?

you could use the EN1PORT maybe to switch displays.

but usually the displays wont hold an image, so NO it wont show different images

Carlos Camacho
Associate
Posted on May 29, 2018 at 15:40

Yeah same image in both displays, they will be about 5cm away from the control board.

The important thing is if this board is able to have two video inputs (HDMI and CVBS) to be passed to the screens.

Posted on May 29, 2018 at 16:34

This is something that I recommend to discuss with your local ST rep and FAEs. There might be solutions, but terminating a bidirectional 500 MHz signal in multiple places doesn't strike me as viable.

There might be hub/switch type DSI/HDMI implementations that provide support for multiple screens or output methodologies.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 29, 2018 at 16:11

I don't think that the STM32 would be able to capture your CVBS signal nor the HDMI signal.

try the Rk3399