STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART interrupt lost

Under FREERTOS on UART3, I receive a 40 byte packet every 2.5ms @ 921600 baud . I programmed the Rx FIFO to interrupt at 1/2 level threshold. Everything works fine for about an hour. Then, for some reason, I get an overrun condition which seems to me...

DMose by Associate
  • 1013 Views
  • 1 replies
  • 0 kudos

STM32F072C8 CANBUS Loopback working but Normal mode isnt.

Hi I am hoping someone can help me with a frustrating problem. I have two boards setup with STM32F072C8 parts. I have downloaded the examples from ST which are for a larger footprint part and modified the code to run on the 48 pin parts. The loopback...

r9rej by Associate
  • 839 Views
  • 0 replies
  • 0 kudos

execution time-STM32F429zi

i am just executing a for loop of 4096 time. But it takes more than 1 ms in stm32f429zi series. Clock frequency is 180MHz. How it can take that much time or whether it is executing some other function in back end.

SR.6 by Associate
  • 1078 Views
  • 1 replies
  • 0 kudos

Resolved! Application start address can be != start of flash ?

Hello,I need to use the example which boots (jumps) into application in external memory, but with a very slight modification:So that the start address of application can be somewhere inside the flash, not particulary at the start of flash, as it is n...

ranran by Senior II
  • 1443 Views
  • 2 replies
  • 0 kudos

Core peripherals?

Where, in the documentation of STM32 devices, can I find out which optional core peripherals are implemented?

USB FS speed vs USB HS with internal FS Phy with DMA

I have a custom board using a STM32F446RET6 with a SDCard. It is configuredbe a mass storage device and use USB_OTG_FS. I read another post where someone mentioned the STM32F4 can use USB HS but usethe Internal FS Phy. The advantage to doing this is ...

STM32H7 -FMC - LCD INTEFACE - A19 AS REGISTER SELECT

Hi, When A0 is used as Register select in the FMC LCD interface, ST uses the code below: typedef struct{ __IO uint16_t REG; __IO uint16_t RAM;}LCD_CONTROLLER_TypeDef;/* We use BANK1 as we use FMC_NE1 signal */#define FMC_BANK1_BASE ((uint32_t)(0x...

Asantos by Senior
  • 1244 Views
  • 4 replies
  • 0 kudos