User Activity

I want to read and write EEPROM in STM32L051K6 microcontroller.
I have to receive a string in stm32f030 from USART using LL library through the interrupt.
I want to generate a pwm in complementary mode such that it has following specs:-1.Non inverted pwm has to vary from 0 to 90% cycle2.Inverted pwm reamins in 7% duty cycle3.Inverted pwm and non inverted pwm does not match at any instant4.Both wave doe...
Posted on June 06, 2018 at 07:57I want to generate center aligned pwm in stm32f030k6tx but when i am chosing the option of  center aligned in counter mode than it is converting it in edge aligned mode.So can any help me in how to generate central al...
Kudos from