STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

usb bootloader

Hi(All?) my nucleo board(s) is/are detected as a USB device in windows. I can drag and drop a firmware binary on them. And the Firmware is automatically updated after power cycling the board. I want to design my own board and use the USB to update t...

PWM on TIM1 CH1 of NUCLEO--F303RE does not start

Hello,I dont't know why in my projetc the PWM daoes not start.I would generate a PWM with Duty =50% and Period =10msec. I use a NUCLEO--F303RE.I started with CubeMX to generate the project configuring IO (blinking the green LED) and the PWM on TIM1 C...

MCere by Associate
  • 2828 Views
  • 5 replies
  • 0 kudos

Nucleo l476RG. Reset when connect to laptopusing usb

Hello.I have a nucleo powered with external 5V. I use to log info using usb.Eache time i need to talke a log to the log, i cannoct my laptop and MCU reset.Anyone know if i can hovoid this? Remove SB12 could help Me? any other hint?Regards,Carmelo

stm32f4 by Associate II
  • 2619 Views
  • 5 replies
  • 0 kudos

Why do GP14 and PB15 GPIOS not work for me?

All other GPIOS work but these two do not. They get the same voltage as the rest (0 and 3.2V). All pins Vdd and Vss I have them well except pin 97 VDD_USB that by mistake I have connected to GND.I have attached the project with which I have been test...

FFran by Associate II
  • 1950 Views
  • 6 replies
  • 0 kudos

Resolved! Question about PC13,PC4,PC5

Hi,Masterplatform:stm32f030C8TxI saw the data sheet as described below:My schematic is as follows:These LED lights can be lit at the same time, the program can also run normally, but their current sum has exceeded 3ma. Although it violates the descri...

0690X000006CqQsQAK.jpg 0690X000006CqQxQAK.jpg
lyu by Associate II
  • 1973 Views
  • 3 replies
  • 0 kudos

Resolved! (SOLVED) STABIP in STM32F373CC never gets cleared

Hi there,I am using the STM32F373CC in LQFP48 package on my own application (not a nucleo or discovery board) with all supplies and references connected to 3.3V and decoupled as suggested by ST.The microcontroller is running as expected, I/Os are ope...

TThan by Associate III
  • 1716 Views
  • 2 replies
  • 0 kudos