STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32l1xx adc is giving random data after conversion done

hi,we are trying to measure vrefint using adc of stm32l1xx. the converted data is keep on varying between 0 to 3000 (decimal). we are not sure where is the problem. can anyone help on this issue? here is the sample code: //hsi clock is enabled in st...

es.18 by Associate II
  • 2302 Views
  • 4 replies
  • 0 kudos

Resolved! Where is pin Nr 1?

Hello,On this picture, which is the pin Nr 1?Top right or bottom left ?ThanksJulien

JulienD by Senior
  • 2263 Views
  • 4 replies
  • 0 kudos

Resolved! How can we use RS-485 in full-duplex ?

Hello,We need to use RS-485 in full duplex, and with the flow control (DE).Is it that when we configure DE with RS485 is shall be used as half duplex ?can I configure rs232 pins with RTS (instead of DE) before converting voltage to rs-485 levels ?Wil...

ranran by Senior II
  • 10297 Views
  • 16 replies
  • 0 kudos

Resolved! STM32H7 SPI ISSUE

Posted on April 06, 2018 at 16:43 Hai, Iam using the STM32H743VIT controller , We are using the spi4 in our board ,we generated the code using the cube mx nothing is coming(CLK and SIN)when transmit the data using the function ( HAL_SPI_Transmit(SP...

MANISH by Associate II
  • 5134 Views
  • 10 replies
  • 0 kudos

internal temperature sensor stability

Hi guys and girls!I'm using STSPIN32F0, an MCU with built-in 3-phase motor driver and I'm trying to read internal temperature sensor. What I'm getting back looks to me like random walk within range of about 10 degrees Celsius (please see attachment)....

Misha K by Associate III
  • 2425 Views
  • 3 replies
  • 0 kudos

Indeterminate state of MCU

We use STM32412 for our battery operated system.A strange case is observed where MCU stopped responding.Neither it got powered up, also seems the code was not being executed.Our NRST pin is powered by the same source by which MCU is powered, so NRST ...

PChan.17 by Associate II
  • 3604 Views
  • 6 replies
  • 0 kudos

get the timer count

Hi,I dont know whats wrong with my code, I just want to test the timer's working .the purpose of the program is to turn off the led after a number of cycle . but this have never been happen, the led still on.PS im working wit HSI_VALUE  ((uint32_t)16...

mmed by Associate III
  • 8425 Views
  • 9 replies
  • 0 kudos