cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4xx_DSP_StdPeriph_Lib_V1.8.0: Incompatible change regarding I2C, Intended or bug ?

AlexKern
Associate II

STM32F4xx_DSP_StdPeriph_Lib_V1.8.0

stm32f4xx_i2c.c : 451

void I2C_Send7bitAddress(I2C_TypeDef* I2Cx, uint8_t Address, uint8_t I2C_Direction)

{

/* Check the parameters */

 assert_param(IS_I2C_ALL_PERIPH(I2Cx));

 assert_param(IS_I2C_DIRECTION(I2C_Direction));

  Address <<= 1; //<---- was here in V1.6.0 but missing in V1.8.0.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0