STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Oscillator calculation STM32

I want to use a STM32F103, STM32L431, 451 and 471 microcontroller, but i don´t know if the crystal that i selected (ABS07-120-32.768kHz-T and ABMM2-8.000MHZ-E2-T) is valid for this microcontroller.And another question is how to calcule the load capac...

Problem with the RCC LSE STM32L496RET6 MCU.

Hello! I use CubeMX to generate the init code for rcc whith LSE Crystal NX3215SA-32.768KHZ-EXS00A-MU00525 (32.768K,6PF), two 2.7pF capacitors and rtc module. Program goes to error handler after "if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)"-s...

RAkma by Associate II
  • 2983 Views
  • 6 replies
  • 0 kudos

How to drive the emmc chip in stm32l4r5 ?

hello. I am an embedded software engineer from China ,At the moment I'm tryingDrive emmc on stm32l4r5 ,but I failed .Who can give me a demo about how to drive emmc on stm32l4xx , thank you​

ydong by Associate II
  • 1967 Views
  • 6 replies
  • 0 kudos

IAP over GSM: UART and Flash programming

Posted on January 07, 2016 at 16:29 Hi, I'm developing an IAP application for firmware upgrade over GSM network. I've a SIM800H module connected to STM32 over UART interface and I'm able to establish GSM connection, setup HTTP GET request an...

gmate1 by Associate II
  • 5911 Views
  • 13 replies
  • 0 kudos

MCU selector misses Voltage reference buffer

Hello,looking for a STM32 in small package with pins where optical solder inspection is possible, I hoped that the MCU Selector from STCube would offer me a checkbox to select devices with Voltage reference buffer output. I did not find that checkou...

how dose the PC run to startup.s when the mcu reset

Hi,dear enginner:  i want to know how the PC run to startup.s when mcu reset?  The Definitive Guide to the ARM Cortex-M3 says address 0x00000000 is MSP‘,address 0x00000004 is ResetVector.  But when I look at STM32F767, I find that 0x00000000 and 0x4 ...

xshen by Associate II
  • 1699 Views
  • 3 replies
  • 0 kudos