STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F4 CRC32 algorithm headache

I am developing a serial comms protocol between two STM32F407s.I am using the hardware CRC module to generate checksums for some of the data.I am also writing a test script in python to aid development.All has gone well until now.Now I need my test s...

AT38 by Associate III
  • 9157 Views
  • 8 replies
  • 1 kudos

Is it possible to use this external SDRAM to store program variables instead of using MCU onboard RAM using the Flexible memory controller (FMC)?

Hi.I am using the STM32746G Discovery Board and running the STemWin which uses the external SDRAM [Part No.: MT48LC4M32B2B5-6A, Manufacturer: MICRON] to buffer the LCD rendering. Is it possible to use this external SDRAM to store program variables in...

Composite Devices Support

Hi there,i wondered if it's possible to support more than two composite device classes. I am using stm32f407ig and in the reference it says there is a control endpoint 0 and it supports 3 IN/OUT Endpoints. So it must be possible to implement CDC+HID+...

arduo by Senior
  • 1153 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F746NG : Output Compare Interrupt triggering at random

I am trying to use Timer Output Compare on STM32F746NG with the following code:void TIM1_CC_IRQHandler(void) { volatile uint32_t a = TIM1->CNT;   printf("DUMMY\r\n"); }   void timer_start(void) { TIM_HandleTypeDef htim1; TIM_OC_InitTypeDef tim1...

APete by Associate II
  • 2333 Views
  • 4 replies
  • 0 kudos

Resolved! System clock is abnormal during stm32f401 using TIM2.

Hello,I am using timer as stm32f401.​However, the clock set in CubeMx is different from the actual clock. (I set it to 48Mhz, but I get 2Mhz when measuring with an oscilloscope.)​I used the MCO pin to measure the PLLCLK clock, but my set clock does n...

SWoon by Associate II
  • 2152 Views
  • 4 replies
  • 0 kudos

shutdown mode concept question

I read that when entering shutdown and waking up through a wakeup pin, the program restarts. If I enter the shutdown in my main method, doesn't that mean that when my MCU wakeup it will restart and then enter the shutdown again in my main method?