STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART with 7 data bits

Hi all!I am using STM32F427 with HAL. I have to communicate with other devices using communication protocol over RS-232 interface (USART). The protocol is using 7 data bits, odd parity. I am struggling to make it work. There is a setting for WordLeng...

Trouble Getting Peripherals to Work... At All

I have a custom board based on STM32H753. It has SDRAM, SD card slot, a couple of I2C peripherals, some GPIOs going to LEDs and a handful more that go to CPLDs which interface to another part of the system.I am not using generated HAL code or CubeMX ...

GSell by Associate
  • 1123 Views
  • 1 replies
  • 0 kudos

Programming arrays of STM32 MCUs

Still struggling with this so hopefully somebody can help me. As far as I can work out the STM32(H7s if it matters) need three pins (TCK, TMS & NRST) plus a common ground to be programmed from another MCU. I can't dedicate three pins on the master ...

MikeDB by Lead
  • 2194 Views
  • 9 replies
  • 0 kudos

STM32H750 in Europe

Are these parts US only?? I need 4 or 5 for prototyping.MOUSER: Will not ship outside USADIGIKEY: Will not ship outside USAST online: $70 postage to Europe. From USA. What else do you expect from a """European""" company.FARNEL : No not stock itRUTRO...

pr242 by Associate II
  • 4638 Views
  • 16 replies
  • 0 kudos

Simple SPI Controller Behavior Question

Am I correct in thinking that an SPI controller in master mode connected to nothing else will send a clock burst whenever it is transmitting?I am troubleshooting an SPI application and it seems as if the master is never transmitting. When I scope SC...

PCROP becoming enabled

We ran a batch of boards with an STM32F401CE on them (this was not the first run of these boards or using this processor).After loading application code, about 10% of the boards became unresponsive. Looking into it we found in the option bytes on th...

BBrie by Associate II
  • 2819 Views
  • 6 replies
  • 0 kudos

STM32H750 SAI interfaces

It was suggested I look at this part as it's definitely superior to the F730. However I can't see how to use the SAI4 interface because its SCK_A and SCK_B pins are shared with those of SAI1. Am I missing something or does this preclude using both ...

MikeDB by Lead
  • 1645 Views
  • 2 replies
  • 0 kudos

Resolved! Reset line pulled low for no reason

I have created my own board based on the STM32L073RZ where I copied certain bits from the NUCLEO borad. I am having a problem where I can't connect to it using the STLINK. I have found out that even with only power plugged in the reset line is pulled...