STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What to do if an LPTIM takes too long to wake up STM32L476 from Stop 2 mode for the first time after every reset when LPTIM1 is used as a Timeout wakeup unit?

I am using STM32L476.I want to enter the Stop 2 mode and use LPTIM1 as a Timeout wakeup unit.The code is written such that the LPTIM1 wakes up the MCU from Stop 2 mode after every second. The LPTIM1 takes too long to wakeup the MCU for the first time...

HShah.14 by Associate
  • 1687 Views
  • 2 replies
  • 0 kudos

lin software on STM32F103 - Detecting stop bit errors

I develop an own LIN slave node software stack for the STM32F103RB. This stack has to pass all tests from the LIN Conformance Test (according to ISO 17987-6). This test is a customer requirement.Actually the software and/or the hardware could not det...

fehrlest by Associate
  • 1297 Views
  • 1 replies
  • 0 kudos

Enter and Exit Low Power Sleep Mode?

Hi,I have configured MCU in Sleep Mode, I have Configured SPI,UART and Some GPIO. and also configured Interrupt RTC. I have Wrote entering Sleep mode like,main(){  MX_GPIO_Init(); MX_LPUART1_UART_Init(); MX_SPI1_Init(); while(1) { Disable_Pheripheral...

STM32G4 ADC clock

Hi, Most of the STM32G4 CubeMX examples configure the ADC clock as synchronous clock mode divided by two,and the AHB ADC bus clock as 150MHZ. If I understand correctly, the ADC clock would be 75 MHZ for this configuration. The problem is that STM32G...

Asantos by Senior
  • 800 Views
  • 0 replies
  • 1 kudos

STM32 I2C Multi-master problem

I'm seeing a problem which seems to be related to the one discussed here: https://community.st.com/s/question/0D50X00009XkgoYSAR/stm32-i2c-multimaster-hardware-bug In my case though I'm not using DMA, I'm just using interrupt driven I2C but the sympt...

SGars by Associate II
  • 1709 Views
  • 1 replies
  • 1 kudos