STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can not open source input file: No such file or directory

Dear friends,I get a silly error " No such file or directory " in Keil IDE while I've already added the file path to include path directory of the compiler.This error happens only when I add lwIP source files to my project. And what's surprising is ...

0690X00000D8VEgQAN.png 0690X00000D8VEqQAN.png
Mujtaba by Senior
  • 4643 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L433 LL SPI sending too much data (16 instead 8)

Hello. I need ability to send only 8 bit at the time. And I can't figure-out why I can send it, it keeps generating 16clocks no matter what LL_GPIO_ResetOutputPin(GPIOA,LL_GPIO_PIN_4); Delay(0x8); while((SPI1->SR&SPI_SR_TXE)!=SPI_SR_TXE); ...

Linas L by Senior II
  • 1655 Views
  • 4 replies
  • 0 kudos

STM32H7 SDMMC IDMA write multiple blocks error

Dear all,I am working with the sdmmc lib from STM and i am trying to get it working in DS (Default Speed @25Mhz) with a CARD_SDHC_SDXC, CARD_ULTRA_HIGH_SPEED sd card.When I write multiple blocks with the IDMA for the first time it’s no problem and ev...

STM32F411RE UART not working with IAR debugger

I am currently learning to work with stm32f411re. I use PA9/10 as TX and RX with baud rate 9600 and 1 start 8 bit word and 1 stop without parity. I connected PA9/PA10 with FTDI to my PC and i am trying to send from serial terminal. Trying to do this ...

AVuji.1 by Associate
  • 1617 Views
  • 3 replies
  • 0 kudos

I am working on NUCLEO-F103RB (target STM32F103RB) with Keil uVision5. What I want to do is to trigger ADC1 injected group with TIM2 CC1 event every 10 microseconds, but it not work. Could anyone help me ?

I have written ADC1_2_ IRQ Handler ISR and TIM2_IRQHandler. TIM2_IRQHandler is executed but ADC1_2_IRQHandler it is not executed.I have also tried to trigger ADC1 injected group with JSWSTAR event and it works fine (ADC1_2_IRQHandler is executed).The...

Silvano by Associate II
  • 891 Views
  • 0 replies
  • 0 kudos

STM32L476 HAL_QSPI_Receive_DMA() hangs intermittently.

While doing heavy activity with a NAND flash, the code is generally working, but occasionally I get hung up waiting for an operation to finish. I trapped it on the logic analyzer several times, and it's never at the same time. In every instance the ...

0690X00000Bvi37QAB.png 0690X00000Bvi2TQAR.png 0690X00000Bvi3RQAR.png
MMitc by Associate II
  • 4938 Views
  • 8 replies
  • 0 kudos