cancel
Showing results for 
Search instead for 
Did you mean: 

Is STM32F44 supports 4Gb DDR4 SDRAM

Predd.11
Associate II

I need to interface 4Gb DDR4 SDRAM with stm32f446vet6 controller

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
waclawek.jan
Super User

The 100-pin package does not have the FMC_SDCLK pin so it does not support SDRAM.

STM32 don't support DDR at all, only SDR.

JW

AVI-crak
Senior

Good joke.

Thanks for the information

is there any possibility to interface SDRAM DDR with STM32F44 without using FMC

There's no reasonable way I know of to interface DDR SDRAMs with STM32.

JW

thanks sir,

Howmuch SDR SDRAM memory (maximum) can we interface by using FMC of STM32F446VE controller?

As I said above, the 100-pin package does not have the FMC_SDCLK pin so it does not support SDRAM.

For larger packages the limit is given by FMC itself; look at the FMC chapter in RM.

JW