STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Using SysTick causes reset?

UPDATE: The issue has been solved. The nBFB2 option bit had to be enabled.Hello, I am currently programming and STM32L152RE on a Nucleo development board. I am using SysTick as a .5s timer that ran a status LED. Everything was working up until recent...

SBona.2 by Associate II
  • 5888 Views
  • 10 replies
  • 0 kudos

Resolved! Read Parallel display commands with STM32

Hi, is it possible to connect STM32 instead of display and read its pins (A0, RD, WR, D0, D1, D2, D3, D4, D5, D6, D7) to know what device is sending and maybe replace original display with different display?For example I would need to detect that WR ...

JBond.1 by Senior II
  • 8268 Views
  • 14 replies
  • 0 kudos

Does stm32f767zi support 3 CANs as slave?

in STMCubeMX it says that CAN1 and CAN3 are master and CAN2 is slave. I need to use all three CANs as slave.Would it be possible to do that? If i can do that would i just be configuring the CAN1 and CAN3 as master in STMCubeMX and continue to use the...

ARam .1 by Associate
  • 993 Views
  • 1 replies
  • 0 kudos

STM32G4 PLL documentation errors

Hi,The documentation between the STM32G4 RM0440 Rev 3 and between the individual MCU specifications is inconsistent when it comes to the PLL limits. In the documentation for RCC_PLLCFGR we have the following two statements:PLLN: "The software has to...

STM32f4 HAL library

Hi, I am using the STM32F4. Now i learning to use the HAL library so i want to ensure i got the same result with and without using the HAL library but now i face some problem.I used the HAL library to control the LED by press the button it is work.vo...

Cl.1 by Associate II
  • 2257 Views
  • 3 replies
  • 0 kudos

Usage of SPI with 16-bit data

Hello,I am using STM32F767ZI with a motor driver from TI (DRV8908) which works via SPI in 16-bit mode and with 5MHz and has the following requirements:1. SCLK pin should be low when the nSCS pin transitions from high to low and low to high.2. nSCS pi...

NJ by Associate II
  • 1070 Views
  • 0 replies
  • 0 kudos

Hi, for several days now I have been trying to display a variable in "Snapshot acquisition mode" in STM Studio. The document CD00291015.pdf talks about this mode on page 21, talking about the "softTrace" subdirectory and the DataAcq.c and DataAcq.h files

Hi, for several days now I have been trying to display a variable in "Snapshot acquisition mode" in STM Studio. The document CD00291015.pdf talks about this mode on page 21, talking about the "softTrace" subdirectory and the DataAcq.c and DataAcq.h f...

Mbert.1 by Associate II
  • 1082 Views
  • 0 replies
  • 0 kudos