STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How do I configure the pullup on GPIO_PIN 6 for STM32G031J6

Problem is that the voltage does not rise to 3.3V, I measure it at 1.64V. The pin has nothing connected to it and I tried this on 2 MCUs.Using STM32CubeIDE 1.2.0 Build: 5034_20200108_0926, I created a simple project and configured pin PB6 as GPIO_INP...

Radiofan by Associate II
  • 8916 Views
  • 12 replies
  • 0 kudos

Resolved! Do STM32F401 and F411 have a CCRAM ?

The documentation of these specific MCU do not show the CCRAM in the memory map.From my understanding this is Cortex-M4 related...https://github.com/ObKo/stm32-cmake/issues/134#issuecomment-651631813

HPhar.1 by Associate
  • 1453 Views
  • 1 replies
  • 1 kudos

PWM+DMA behavior differes on STM32F407 compared to STM32G474

I tried to generate a 2-channel PWM on both the STM32F407 and the STM32G474. I was surprised to see that the PWM of both channels started simultanously, while for the F4 there was a delay. Is this intended behavior? Is there a work-around?This is fro...

0693W000001s6UOQAY.png 0693W000001s6QXQAY.png
AShri.1 by Associate II
  • 1467 Views
  • 0 replies
  • 0 kudos

memcmp crashes when accessing data stored in flash

STM32H745ziI am storing some configuration data in flash memory at address 0x080E0000.If I call HAL_FLASHEx_Erase and then do a memcmp of 24 bytes at this address vs a buffer where I have prepared data I want to write there everything is fine althoug...

KWest.1 by Associate II
  • 2343 Views
  • 3 replies
  • 0 kudos

Resolved! i would like to know how linker commands can be used in source file to push the multiple structure defines into a part of code memory. can some body share with examples

steps i tried.step 1: created a section in linker file ".parambuf"step2: in source file declared a structuretypedef struct{ param_t param[256]; \} t_param_block_t;step 3: in header files using attributes commands to push into parambuf section.extern ...

Anand Ram by Associate III
  • 1219 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F7 + QSPI (QUADSPI): Sporadic failure with memory-mapped flash memory. Disabling timeout does not help.

Hi everyone,We have an issue when using QUADSPI (memory-mapped) on a STM32F7 microcontroller. The controller sporadically runs into a watchdog reset. Investigation showed that the crash always occurs during a LDM instruction from the memory-mapped fl...

auraner by Associate II
  • 4776 Views
  • 6 replies
  • 0 kudos

Resolved! What STM32 Microcontroller will fit me

I am trying to make the transition from Arduino/Atmel micro controllers to something that can support true threading/multitasking in the 32bit ARM processor category. I am making a robot where I need to control 7+ 12v motors, 24 servos, 100+LEDS, spe...

ENoot.1 by Associate II
  • 6267 Views
  • 6 replies
  • 0 kudos

Problem Porting TLS CLient from F207 to H743

I managed to get a simple TLS client working on the NUCLEO-F207ZG. I cannot get the program to run on the NUCLEO-H743ZI2. On Wireshark I see several DHCP DISCOVER messages go out; followed by an OFFER message coming back. My code never responds with ...