STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can't run any samples for NUCLEO-L011K4 board

I have a NUCLEO-L011K4 dev board, and unfortunately I can't get any of the sample programs to work. The board doesn't show up on the host machine. I'll walk you through the steps I tried on Windows, but I also on Mac and it didn't work there either:I...

0693W000003BI4jQAG.jpg
ZRatt.1 by Associate II
  • 2031 Views
  • 4 replies
  • 0 kudos

STM32F401RE UART Interrupt

Hello, I'm new to embedded software and I have 2 questions about UART communication.I've coded UART interrupt and have no problem with the transmit function, but the HAL_UART_Receive_IT(&huart2, rx, 10);only read the first byte I passed to the serial...

Kabeone by Associate
  • 1598 Views
  • 3 replies
  • 0 kudos

Resolved! External RAM on STM32H743IIT6

I am trying to set up FMC to work with external RAM. The code compiles and works with KEIL, but I am trying to make it work with STM32CubeIDE. The code compiles and runs, but the RAM is not initialized. I copied all of the code, including the .ioc fi...

GGowi.1 by Associate II
  • 8477 Views
  • 18 replies
  • 0 kudos

Function for printing values

Hello,I'm working with the NUCLEO-F722ZE EVB on STM32CubeIDE.I want to use the main USB connection to the PC as a UART.The default CubeMX pin configuration already has PD8 and PD9 configured as a UART, so I proceeded with code generation (the auto ge...

skon.1 by Senior
  • 9247 Views
  • 13 replies
  • 0 kudos

Cycle counter accuracy with PLL and HSE Clock for STM32L4

I am currently designing an application where I will read Sensors that can be integrated over time (e.g. Accelerometer, flow meter). As a first step I want to calculate whats the maximum error I could get by using the cycle counter as a unit of time....

VChav.19 by Associate II
  • 3195 Views
  • 4 replies
  • 0 kudos

HAL_UART_Receive doesn't block execution

Helllo,I'm working on the NUCLEO-F722ZE EVB.I want my code to wait for a character to be received from UART 3 and do nothing.This is what I wrote:unibt8_t received_character = 0 ; HAL_UART_Receive(&huart3, received_character, 1,1000) ;From what I und...

skon.1 by Senior
  • 5228 Views
  • 9 replies
  • 0 kudos