STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DS12288 Rev 5 - Missing Figure in section 5.3.14?

On page 130, just above Figure 25 the paragraph references Figure 25 twice. Either there is a missing figure or there is an extra reference.The coverage of these requirements is shown in Figure 25 for standard I/Os, and in Figure 25 for5 V tolerant I...

configure uart or swv (bluecoin) STEVAL-BCNKT01V1

hi everyone i am using an example audio loop example and planning to print the variable called pcm buffer on to console either swv or using the pins on the bluecoin station as uart pheripheral how should i implement this or worst case how to implemen...

Generate fixed number of pulses in stm32F446ME

Hi,I am using STM32F446ME controller to monitor the LI-ion battery(STBC02) status. I need to provide the pulse number as 9 with start and stop bit with time characteristics to initiate the battery to monitor the voltage level. I am using TIM1 for thi...

KSakt.1 by Associate
  • 1301 Views
  • 1 replies
  • 0 kudos

How can I accept N IDs on CAN?

I'm trying to filter all IDs except 4 using the struct "FDCAN_FilterTypeDef", without using "FDCAN_FILTER_RANGE", "FDCAN_FILTER_MASK" but a type like "FDCAN_FILTER_DUAL" not with DUAL but N.How can implement it?

FScat.1 by Associate
  • 640 Views
  • 0 replies
  • 0 kudos

STM32 F4 - SDIO - Facing Data CRC failure while doing SDIO read/write, Anyway to avoid or recover this problem?

Hello!I am using STM32-NUCLEO-F412ZG board. I want to use SDIO (only IO) functionality as host.I am able to init, read, write to SDIO peripheral using polling.Before asking question let me give some background of implementation,Not using DMA4 bit SDI...

0693W000008ztvLQAQ.png
YMant.1 by Associate II
  • 1585 Views
  • 1 replies
  • 0 kudos

VREF+ Pin on STM32F103RCY6 (WLCSP64 Package)

I have a question regarding the VREF+ Pin in the above mentioned device. The datasheet DS5792 Rev 13 of the STM32F103xC devices states on page 36: " Unlike in the LQFP64 package, there is no PC3 in the WLCSP package. The VREF+ functionality is provid...

UART DMA TX

Hi there !Is the first time i wrote at this forum. I start to work with UART and DMA ,and i configurate the buffer in circular mode. I don't understa why when i call the library he continus to send over and over all i have in the buffer , i appearanc...

SGian.1 by Senior
  • 1444 Views
  • 3 replies
  • 0 kudos