cancel
Showing results for 
Search instead for 
Did you mean: 

Hi. I have a query, related to the global interrupt of the Uhart. Is there any way we can enable more than one interrupts for a singal uhart.

Kkhan.2
Associate

Actually I am using a single interrupt to receive, data from another processor in two different arrays. Due to this scenario and interrupt being called at two times in different arrays, only the first array receive interrupt accurately.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

Each typically has a single vector but can handle multiple sources within the USART.

If the Vector Table is in RAM you can dynamically change the subroutine called.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Kkhan.2
Associate

Kindly explain completely about RAM dynamically subroutine function

There are Technical Reference Manuals for the MCU, a review of those might be enlightening.

Have a sufficiently large 32-bit array​ to hold all the Vector entries, have it on a 512-byte aligned address. Copy the current defaults into this new array. Point SCB->VTOR at this new array.

C​hange the function address pointer in the array index for the USART interrupt.

I​f this is too complex, perhaps use a function pointer your IRQ Handler calls.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..