STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

After relocating IVT using VTOR, application work only in DEBUG session but not without debugger or Programmer (flash Hex file)

Hello,I am using sample program RTOS Thread creation with LED toggling for STM32H723 nucleo board.LED toggles and application works properly with interrupt vector table at default Flash address 0x0800.0000. This works for debug session. This also wor...

VJAIN.1 by Associate
  • 11693 Views
  • 3 replies
  • 0 kudos

Modbus rtu on STM32L031G4

I want to implement the modbus rtu on the micro STM32L031G4 which library do you recommend?(if you use freeROTS how should I configure the micro da cube ide?)

Fscu.1 by Associate II
  • 5823 Views
  • 2 replies
  • 0 kudos

Set sdcard "temporary write protect" bit - STM32f7

Hi.I'm working on a project with a STM32F722 and a microSD card. I'm using HAL_SD & FatFS.I want to modify the CSD of the SD card to set the "temporary write protect" bit to 1, to protect the card from accidental writes.It is my understanding you can...

TGeof.2 by Associate II
  • 2193 Views
  • 1 replies
  • 0 kudos

Resolved! How can I use Vdda/Vref pin to get better range for ADC

Hello. I need STM with external Vref 3V. But I don't need so much pins like 100pins in ST where we have special pin Vref. Could I use VDDA/Vref pin in STM32F103RC according to drawing belloow? I wanna connect precision voltage reference to VDDA on 3...

RGima.1 by Associate II
  • 8100 Views
  • 4 replies
  • 0 kudos

Resolved! LSE vs LSI for periodic wakeup from Stop

Does LSE have any power-saving advantages over LSI when the RTC is used to periodically wake up from low-power modes? Or does it just provide better accuracy for the RTC? For example, let's say you only use the RTC to wake up from stop mode, but neve...

DOCon.1 by Senior
  • 3820 Views
  • 2 replies
  • 0 kudos

STM32F103 timer interrupts with HAL_TIM_PWM_PulseFinishedCallback and HAL_TIM_PeriodElapsedCallback does not work as intended

I am trying to do a blink example for testing using built-in LED on bluepill. Unlike regular delay and period interrupts, i want to try a custom-duty blink, in which i want 3s on and 2s off, a total of 5s period.in main: HAL_TIM_Base_Start_IT(&htim1)...

MKanc.1 by Associate III
  • 1433 Views
  • 2 replies
  • 0 kudos

Resolved! Note about use of real name on this ST community forum

(edited this post from previous panic language; still think its good to keep it around - and a suggestion: there should be a tag/category for "Community Website")Well, since ST asked me to register for downloading software, I thought I'd be honest, a...

0693W00000AMpBnQAL.png 0693W00000AMpKBQA1.png
sdbbs by Associate II
  • 1520 Views
  • 2 replies
  • 0 kudos