STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Migrating from L4 to F4

What are the main points which I have to consider when migrating from STM32L4 to Stm32F4 apart from the connecting peripheral power management, Is there any main points which I have to consider when programming.

Roshan by Associate III
  • 2109 Views
  • 4 replies
  • 0 kudos

What's the difference between STM32L4S5ZI and STM32L496RET?

Hello, I just wanted to ask is there a big difference between STM32L496RE and STM32L4S5ZI. Other than STM32L4S5ZI having a larger RAM and memory. As well as no display interface but with encryption. I'm asking because the STM32L496RE is now out of st...

HAhme.1 by Associate II
  • 1626 Views
  • 2 replies
  • 0 kudos

How to Turn ON the STM32 with button?

Hello!I have a question about power supply and ON/OFF capabilities of microcontroller.Normally, When power supply is turned ON, the microcontroller Start executing the program.In my case I want that after Power supply is turn ON, the microcontroller ...

DIvan.1 by Associate III
  • 4519 Views
  • 5 replies
  • 0 kudos

Resolved! How can I use Capture Compare as external trigger source?

Hi!This might be a simple question, but I still haven't solved it. I want to create an external trigger source for SDADC 16-bit and I have selected TIM12 Capture Compare 1 as external trigger source. Then I have enable the Output Compare, because I d...

0693W00000BbUBbQAN.png 0693W00000BbUBgQAN.png
DMårt by Lead
  • 3515 Views
  • 5 replies
  • 0 kudos

Unable to read from ADS8686S properly via SPI

I am trying to read registers from an ADS8686S ADC from TI. It has the following timing diagram for register reads (from https://www.ti.com/lit/ds/symlink/ads8686s.pdf?ts=1624204868114&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FADS8686S):...

0693W00000BbTiKQAV.png
JRest.1 by Associate
  • 1654 Views
  • 1 replies
  • 0 kudos

How to implement remap function in STM32L5

Hi,Because the STM32l5 not support "__HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH", Please tell me how to change the program entry point without program on-chip flash.ThanksQiZhang"void AppEnter(){ #define SYS_MEM_ADDR 0x8020000 __HAL_SYSCFG_REMAPMEMORY_SYSTE...

zqizh.1 by Associate III
  • 711 Views
  • 0 replies
  • 0 kudos