STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IWDG watchdog timeout even refresh it

I have a customized bootloader and a main application.Both of them init the wathcdog, and refresh it. But when my bootloader jump to application, the refresh of watchdog from application sometime does not work. The watchdog still timeout.But if run t...

jiangpen by Associate II
  • 1265 Views
  • 1 replies
  • 0 kudos

High accurate sine wave using STM32H7

Hello,Is it possible to generate high accuracy in terms of the frequency sine wave using STM32?My goal is to generate a sine wave using STM32 whose frequency varies from 5KHz to 20KHz insteps of 0.1Hz with a delay of 1 sec is it possible to use STM3...

GHARI.1 by Associate II
  • 3827 Views
  • 6 replies
  • 0 kudos

STM32 production

When will ST increase STM32 micro-controller production in Europe. For now it is almost impossible to buy STM32 micro controllers?

MCUpwr by Associate III
  • 1777 Views
  • 3 replies
  • 1 kudos

External Flash Loader linker script file

I'm trying to make a custom external flash loader for my STM32F746 uC based board and i found some templates for this purpose from this link that is belongs to the ST workshop on this YouTube link. So when i dug into the corresponding files i saw tha...

ARost.9 by Associate III
  • 6114 Views
  • 9 replies
  • 1 kudos