STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [SOLVED] STM32G030F6 TIM16.1 no output on PB8

I'm trying to get square pulses on PB8 with TIM16.1 output compare, but no pulses on pin (timer seems working: CNT counting, SR flags changing).Setup code:gpio_mode(GPIOB,8, GPIO_MO_AF); gpio_af(GPIOB,8, 2); // PB8 as AF2 rcc_apb2_on(RCC_APB2_TIM16);...

ne562 by Associate II
  • 1800 Views
  • 2 replies
  • 0 kudos

Resolved! EXTI15_10_IRQn triggered constantly - STM32L4R5ZI

Hi, I am trying to write an interrupt code to trigger LED(PB14) using user button on my NUCLEO board(PC13). however, as I observed from the debugger, pending bit for line 13 constantly at 1 without pushing the button at all.The EXTI->PR1 = 1<<13 stil...

KHuyn by Associate II
  • 3177 Views
  • 4 replies
  • 0 kudos

How to change the number of ranks after ADC initialization

I use 6 ADCs.I use 3 channels(Ch1, Ch3, Ch13) for ADC1.I use 3 channels(Ch2, Ch4, Ch15) for ADC2.Use DMA1 Channel1, DMA1 Channel2 respectively.DMA1 Channel1 is used by ADC1,Number Of Conversion is 3, Rank 1 = Ch1, Rank 2 = Ch3, Rank3 = Ch13.​When usi...

STM32G070 And Bme680 help i2c

hi i'm trying to use the bme680 but i can't find any library for it ,plus the datasheet is so confusing if you had any luck using it please help thanks in advance

bakhti by Associate II
  • 2223 Views
  • 3 replies
  • 0 kudos

Problems with I2C register code (STM32G0x1)

I am attempting to write register level code to control the I2C peripheral in an STM32G0x1.My read function is failing because the RXNE bit is never getting set. I believe I have implemented the state machine described in RM0444 (p. 958). Is there ...

SHobb.1 by Associate III
  • 2435 Views
  • 4 replies
  • 0 kudos

I have made a target board using STM32G484VE . I am using 11 ADC pins spread across ADC1 - ADC5. I have introduced a 3.3V Zener BZT52-B3V3 as a protection at all ADC inputs, but all the ADC voltages read 0.6V less from the actual voltage ? Any reason ?

I have made a target board using STM32G484VE . I am using 11 ADC pins spread across ADC1 - ADC5. I have introduced a 3.3V Zener BZT52-B3V3 as a protection at all ADC inputs, but all the ADC voltages read 0.6V less from the actual voltage ? Any reason...

BSUJA.1 by Associate
  • 1684 Views
  • 1 replies
  • 0 kudos