STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CS Glitch with 9-Bit SPI on STM32

Hi everyone,I’m experiencing unexpected behavior while testing 9-bit SPI on an STM32, observed with a logic analyzer. The issue only occurs when the MOSI line is physically connected to the slave.Observations::keycap_1: MOSI not connectedCS and SCLK ...

MOSI connecté.png MOSI non connecté.png
Ameni by Associate II
  • 29 Views
  • 1 replies
  • 0 kudos

Glitch sur CS avec SPI 9 bits sur STM32

Bonjour à tous,Je rencontre un comportement anormal lors de tests SPI 9 bits sur un STM32, observé avec un logic analyzer. Le problème se produit uniquement lorsque la ligne MOSI est physiquement connectée à l’esclave.Observations ::keycap_1: MOSI no...

MOSI connecté.png MOSI non connecté.png
Ameni by Associate II
  • 28 Views
  • 1 replies
  • 2 kudos

STM32C011. Cant run sysclk from LSI.

Im trying to run SYSCLK from LSI on a STM32C011. But it appears as if the MCU is not running. I cant see anything in the datasheet that says the clock cant be used and it can be routed fine in the clock configurator. Am I missing something in the dat...

SHDK2000 by Associate II
  • 484 Views
  • 28 replies
  • 9 kudos