STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 2 kudos

SysTick_Handler not called, STM32G0B1

I am using CubeIde for the first time.First test - run minimal program with HAL from CubeIDe Configurator, under debuggerSimple program, only SYSTICK and uart , but SysTick_Handler() is not trigged at all .And function HAL_Delay hangs because uwTick...

Xme by Associate II
  • 20660 Views
  • 23 replies
  • 7 kudos

Resolved! Udapte STM32CubeMX

Hello, I have Version STM32CubeIDE : 1.18.0, and I get a program that was communicated to me, but I have this message below :  And I downloaded and installed STM32CubeMX 6.14.1 version, but it seems that it is not taken into account in the environme...

DYann1_0-1745311554144.png DYann1_1-1745311766549.png
DYann.1 by Senior II
  • 1884 Views
  • 4 replies
  • 0 kudos

Resolved! CubeMX 6.14 generate OpenAMP error in STM32H747 error.

Hi all,I am using CubeMX 6.14 to generate an OpenAMP project for the STM32H747I-DISCO board. When I build the project, I receive the following warnings, and it results in an 'OpenAMP create endpoint' error at runtime. I used the same code and project...

Tom17 by Associate II
  • 2896 Views
  • 8 replies
  • 1 kudos

Update STM32CubeMX and STM32Cube MCU Packages

Hello, I want to update STM32CubeMX and STM32Cube MCU Packages, but I can't do because of the error.I tried to run STM32CubeMX in admin mode, but the error occured again.1. How do you solve this error?2. Is 'STM32Cube Updater' a real file? # Error Te...

StrangeTau_0-1744693629582.png StrangeTau_1-1744693678480.png