STM32CubeMX V6.11.0: Migration issue - ADC3 Temperature Sensor Channel missing
- 4 replies
- 3387 views
Target Board: STM32H743ZI2 Nucleo
STM32CubeMX: V6.11.0
Hallo community,
I'm encountering an issue about migration. When I migrated my STM32CubeMX project from V6.10.0 to V6.11.0, the setting for ADC3 was disabled in the new *.ioc files. In my old ADC3 settings, I was using the Temperature Sensor Channel on the chip. But after the update to V6.11.0, the setting for Temperature Sensor Channel in the ADC3 is missing. All the settings of ADC3 for the temperature sensor are missing, and there is no ADC channel 18 under ADC3 to set (The inner temperature sensor is connected to ADC channel 18).
I've also checked the STM32CubeMX 6.11.0 release note and errata. There is no such an issue reported.
I put the two screenshots in the attached files.
Best wishes,