STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

STM32F373CCT6 USB-CDC

I am currently using CUBE MX to set up the USB-CDC function of STM32F373CCT6, but I can't find the VBUS pin. I am using the onboard power supply, and I don't know if I need to use VBUS. If there is a design example for reference, it would be very gra...

AnthonyHu0730_0-1749670403751.png AnthonyHu0730_1-1749670421718.png AnthonyHu0730_2-1749670434327.png

Resolved! NUCLEO-N657X0-Q STM32CubeMX (.IOC) Template

Hello,is there NUCLEO-N657X0-Q template(s) available for CubeMX GUI (IOC project) that is/are preset for XIP or LRun? (ExtMem, Loader, XSPI etc settings ready).I'm trying to build a basic blink project starting from CubeMX IOC with BSP support (that ...

Unfgr by Associate III
  • 756 Views
  • 1 replies
  • 0 kudos

Resolved! Nucleo-U5A5ZJ-Q and RNG code generation

Hello Community,I have a Nucleo-U5A5ZJ-Q development board and have generated code for it using CubeMX (version 6.12.0).  The generated code contains this for the user button:void EXTI13_IRQHandler(void) { /* USER CODE BEGIN EXTI13_IRQn 0 */ /* ...

Resolved! STM32H523CC: SPI2_IRQHandler is never called

Hi,I have a CubeMX-generated code, where I want to receive data from the SPI. Unfortunately, the SPI2 ISR SPI2_IRQHandler() is never called. What I have checked/tried:hardware signals all are there and at the expected pinsinitialisation is done (it i...

add lwip to cmake project for stm32h5

I need to add the LwIP component to a cmake STM32CubeMX generated project for the NUCLEO-H563ZI board.The LwIP component does not appear to be included in the STM32H5 package although the FreeRTOS component is.Is there a way to modify my top level CM...

Unable to open project

After a period of not touching the software.Unable to open a project.Tells me to update software.Existing software 6.9.2Software to update 6.14.1.Doesn't let me check the box.I am an administrator on this computer.How can I open the project and start...

ATfE support

Is there any plan to support creating ATfE-based camke projects in CubeMX?ATfE link: https://github.com/arm/arm-toolchain

JontyLi by Associate II
  • 680 Views
  • 2 replies
  • 0 kudos