STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1574 Views
  • 0 replies
  • 2 kudos

Resolved! SPI-receiver gets out of sync?

Hi,I'm using a STM32H523CC to receive 24 bit data frames via SPI. The SPI acts as receiver-only and is configured as follows:Within my application I do not make use of the HAL-functions but have overwritten the SPI2_IRQHandler(). There I continuously...

Clipboard01.png

Resolved! Starting with X-Nucleo-67W61M1 in CubeMX

I am setting up a project using CubeMX to evaluate the 67W61M1 device, using a Nucleo-F411RE. As far as I can tell the X-NUCLEO-67W61M1 needs SPI1 of the Nucleo for communication. Unfortunately, the Nucleo has SWO (PB3) where SPI1_SCK and while I see...

SidPrice by Associate III
  • 817 Views
  • 2 replies
  • 1 kudos

Resolved! Bug on programming GPDMA transfer (ADC2)

I would like to report a bug, I post it here as so anybody can read it.The bug concerns the GPDMA on STM32H563, but maybe it could happen on others MCUs. I wanted to use a GPDMA1 Channel from a ADC2 request, my Channel was correctly initialized, but ...

Karakala by Associate II
  • 1746 Views
  • 4 replies
  • 1 kudos

CMake project bug in cubeMX6.14.0

On a NUCLEO-H7S3L8 I've been testing the Projects/NUCLEO-H7S3L8/Applications/USBPD from STM32Cube_FW_H7RS_V1.2.0 with cubeMX6.14.0. I use the VScode extension, so I select the CMake toolchain. I select the "copy only necessary files" in code generati...

AEfth by Associate II
  • 1261 Views
  • 2 replies
  • 0 kudos

threadx does not allow BSP code to initialize

with a standard project with only threadx and bsp code added via STM32CubeMX code generates the MX_ThreadX_Init function in main.c but the BSP initialization functions are below this call.MX_ThreadX_Init actually starts the kernel task switching (unl...

mbedTLS with support of TLS_1.3 in STM32CubeMX

Hi,I'm using the STM32H753I-EVAL2 (MCU Type: STM32H753XIHX) to develop a new product.The product will communicate to server using the LwIP (TCP Layer) + MbedTLS (SSL/TLS Layer), running over FreeRTOS environment.We want to use the latest TLS protocol...

APilai by Associate
  • 5964 Views
  • 3 replies
  • 5 kudos

ATfE(Arm Toolchain for Embeded) support

(repeated post)Currently, STM32CubeMX generates CMake projects based on the ARM-GCC compiler toolchain by default. However, in modern STM32 development environments, this toolchain appears to have performance limitations and may no longer fully meet ...

JontyLi by Associate II
  • 1027 Views
  • 0 replies
  • 0 kudos

STM32F373CCT6 USB-CDC

I am currently using CUBE MX to set up the USB-CDC function of STM32F373CCT6, but I can't find the VBUS pin. I am using the onboard power supply, and I don't know if I need to use VBUS. If there is a design example for reference, it would be very gra...

AnthonyHu0730_0-1749670403751.png AnthonyHu0730_1-1749670421718.png AnthonyHu0730_2-1749670434327.png