2023-06-04 2:20 AM
I am trying to use stm32f407 and w25q128 to get a usb drive, for this I wrote a driver to control the flash drive and initialized the USB MSC using CubeMX. When I connect the stm32 to the PC (Ubuntu) I see the new storage device in the Disks app but it doesn't mount, I tried to erase it but the process freezes until I reboot the board
w251128 has:
PageSize = 256
SectorSize = 4096
SectorCount = 4096
PageCount = 65536
BlockSize = 65536
CapacityInKiloByte = 16Mb
Based on this information, I set the defines in `usbd_storage_if.c`:
```
#define STORAGE_LUN_NBR 1
#define STORAGE_BLK_NBR 0x1000
#define STORAGE_BLK_SIZ 0x1000
int8_t STORAGE_Read_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)
{
w25q_readSector(buf, blk_addr, 0, blk_len * 4096); // 0 is offset
return USBD_OK;
}
int8_t STORAGE_Write_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)
{
w25q_eraseBlock(blk_addr);
w25q_writeBlock(buf, blk_addr, 0, blk_len * 4096);
return USBD_OK;
}
```
I added some printfs inside these methods to notify the start and end of the process, if I erase blocks/sectors/pages from the main function in `main.c` everything goes fine, but when I try to erase the flash drive using PC OS and `usbd_storage_if.c` I see that the process just started but never finished, also adding the above code to the read function gives the following popup window "Error wiping device: Failed to probe the device 'dev/-sdb' (udisks-error-quark, 0)".
I also tried to comment out the w25q code and replace it with memcpy to work with internal memory, this works as expected, but how do I use external SPI flash memory as the MSC?
Solved! Go to Solution.
2023-06-04 11:42 AM
Thanks for your reply! Yes, I found the problem. It seems OS doesn’t like delays inside the driver functions. My driver has HAL_Delay() for a few ticks while using spi transmit/receive. When I comment out all delays I got MSC working
2023-06-04 9:23 AM
Test the IO routines thoroughly
Instrument interaction
See what OS is doing when failed.
Make sure sector size and capacity are correctly reported. ie INQURY and READ CAPACITY/MODE PAGE
Can't use FatFS and MSC concurrently, but can use f_mkfs() to format suitably first time around.
2023-06-04 11:42 AM
Thanks for your reply! Yes, I found the problem. It seems OS doesn’t like delays inside the driver functions. My driver has HAL_Delay() for a few ticks while using spi transmit/receive. When I comment out all delays I got MSC working
2024-09-07 3:26 AM
Hi @carlogulliani
Could you please share the code for this? I'm working on same but w25q32 and STM32U0 series MCU. It would be very helpful if you could share the code so that I can use that as a reference.
Regards,
Bharath