STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Uses FreeRTOS functions checkbox in CubeMx

Posted on July 13, 2017 at 10:03Hello there,I am using CubeMx with FreeRTOS for a while now. I am still not sure how does the checkbox ''Uses FreeRTOS functions'' works under NVIC Configuration settings:I would appreciate an explanation on what does...

0690X00000607WyQAI.png

cubemx modify the project properties problem

Posted on April 08, 2017 at 11:03Hi. I'm using STM32CubeMX V4.20.1 and System Workbench for STM32(SW4STM32) now.Actually I use CubeMX plugin for SW4STM32.the problem is...when I click 'Generate Code' after changing the gpios or timers or any changes...

Jisu Kim by Associate II
  • 3331 Views
  • 5 replies
  • 0 kudos

STM32CubeMX USART Limitation/Bug Report

Posted on July 06, 2017 at 19:06Hi. I have noticed that STM32CubeMX has some limitations when configuring a USART for synchronous mode. I am using a STM32F413RGTx running at 100 MHz.I am configuring USART3 for synchronous transmit/receive (pseudo SP...

Resolved! USBD_CDC_INTERVAL not used

Posted on December 06, 2016 at 18:20The define USBD_CDC_INTERVAL in usbd_conf.h generated with CubeMX is not used anywhere in the project. It was used in the old USB Library in the usbd_cdc_core.c SOF-Function, which no longer exists.#f4 #usb #cubem...

CubeMX code for Nucleo32 L432KC does not build

Posted on July 04, 2017 at 18:33Repro steps... Create a new CubeMX project, selecting the Nucleo32 L432KC board.In settings give it a name and select to generate code for the 'System Workbench for STM32' selecting SW4STM32Generate the code and open...

Resolved! CubeMX: Where to place own source/header files?

Posted on June 23, 2017 at 15:24Hey guys,i just created a project for the STM32L4 Discovery Board with CubeMX (I'm using Atollic TrueStudio). I assume that CubeMX always generates the same structure, namely the folders 'Drivers', 'Inc', 'Src', 'star...

STM32F7: Keil Logic Analyzer

Posted on June 17, 2017 at 22:41Hi everyone,I decide to start a discussion about the use of the Keil (v5) logic analyzer with the STM32F7 MCU.For example: in the STM32F7 cube examples there is an interesting example about the ADC capability of the F...