STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 2 kudos

Resolved! FW.F1.1.6.0 Debug in OpenSTM32

Posted on July 19, 2017 at 16:49Hi. I was running CubeMx4.21.0 and upgrade for 4.22.0This meant an upgrade on the F1 family from 1.4.0 to 1.6.0 (may 2017)have a bootloader configured, so debug should align to 0x8004000 On the new version everything ...

DJC by Senior
  • 1155 Views
  • 1 replies
  • 0 kudos

Difference Yellow marker and Red marker in CUBE MX

Posted on July 25, 2017 at 04:35HiWhat is the difference Yellow marker and Red marker in CUBE MX?Can I ignore the Yellow message and use that function?I want to use 6 channel of SDADC, but the Yellow message make me confuse.Is there any problem?i at...

0690X00000607g4QAA.png

STM32F4 with two SDIO

Posted on July 26, 2017 at 05:52I WANT TO KNOW THE STM32F4 SERIES BOARD HAVING TWO SDIO INTERFACES???ANYONE PLEASE SUGGEST ME......https://community.st.com/community/stm32-communityhttps://community.st.com/community/stm32-community/stm32-forumFahren...

Resolved! STM32F030 - Problems with PLL

Posted on July 22, 2017 at 00:59I have been using an STM32F030C6 and configuring it with STM32CubeMX and have had success running the chip using the 8MHz HSI and an external 16MHz crystal. I would like to run at 48MHz but I have not had any luck ena...

0690X00000607dxQAA.png

Set USB Max Power for CDC Device Using STM32CubeMX?

Posted on March 06, 2017 at 01:23I am using an STM32L4 device.  I am making a USB device that uses CDC and have battery charge detection enabled.  I need to request 500mA from the USB port if a standard downstream port is detected.  It appears that ...

cubemx font on high res displays unusable

Posted on August 03, 2016 at 19:57Hi,Recently acquired a laptop with a 3240 x 2160 display running Windows 10.  Some of the dialog boxes and configuration tables are unusable because the fonts used do not fit within the space allocated for the text....

STM32CubeMX V4.21.0 and Java 1.8.0_131 crash

Posted on June 20, 2017 at 17:49Since my last update of WIN10, Java and STM32CubeMX (I did all after Windows update) my STM32 Cube MX crashed on lot of actions : can not load a project, can not save project etc... Any suggestion ? My PC runs WIN10 6...

Vu TRAN by Associate II
  • 4038 Views
  • 5 replies
  • 0 kudos