cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4 HAL_PCDEx_BCD_VBUSDetect() Broken for (non-OTG) USB

Rob.Riggs
Senior III
Posted on July 02, 2017 at 03:41

I am using STM32CubeMX 4.0 and STM32L4 HAL version 1.8.1.

TheHAL_PCDEx_BCD_VBUSDetect() function for 'USB' and 'USB_OTG_FS' differ and the 'USB' version is buggy.

TheHAL_PCDEx_BCD_VBUSDetect() function

is supposed to callHAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DISCOVERY_COMPLETED) when the BCD discovery is complete. However, the way the 'USB' version of thefunction is written, it will only be called when a 'Charging Downstream Port' is detected and not for the other port types.

The code as written looks likethis:

 /* If Charger detect ? */
 if (USBx->BCDR & USB_BCDR_PDET)
 {
 /* Start secondary detection to check connection to Charging Downstream 
 Port or Dedicated Charging Port */
 USBx->BCDR &= ~(USB_BCDR_PDEN);
 USBx->BCDR |= (USB_BCDR_SDEN);
 HAL_Delay(300);
 
 /* If CDP ? */
 if (USBx->BCDR & USB_BCDR_SDET)
 {
 /* Dedicated Downstream Port DCP */
 HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DEDICATED_CHARGING_PORT);
 }
 else
 {
 /* Charging Downstream Port CDP */
 HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_CHARGING_DOWNSTREAM_PORT);
 
 /* Battery Charging capability discovery finished 
 Start Enumeration*/
 HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DISCOVERY_COMPLETED);
 }
 }
 else /* NO */
 {
 /* Standard Downstream Port */
 HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_STD_DOWNSTREAM_PORT);
 }�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

The code should look like this (which is essentiallythe same as the USB_OTG_FS version in the same file):

 /* If Charger detect ? */
 if (USBx->BCDR & USB_BCDR_PDET)
 {
 /* Start secondary detection to check connection to Charging Downstream 
 Port or Dedicated Charging Port */
 USBx->BCDR &= ~(USB_BCDR_PDEN);
 USBx->BCDR |= (USB_BCDR_SDEN);
 HAL_Delay(300);
 
 /* If CDP ? */
 if (USBx->BCDR & USB_BCDR_SDET)
 {
 /* Dedicated Downstream Port DCP */
 HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DEDICATED_CHARGING_PORT);
 }
 else
 {
 /* Charging Downstream Port CDP */
 HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_CHARGING_DOWNSTREAM_PORT);
 }
 }
 else /* NO */
 {
 /* Standard Downstream Port */
 HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_STD_DOWNSTREAM_PORT);
 }
 
 /* Battery Charging capability discovery finished 
 Start Enumeration*/
 HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DISCOVERY_COMPLETED);�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

HAL_PCDEx_BCD_VBUSDetect() must call

HAL_PCDEx_BCD_Callback()

withPCD_BCD_DISCOVERY_COMPLETED without regard tothe port type detected.

Please fix this.

#stm32cubemx #stm32l4 #hal #usb #bcd #pcd
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee
Posted on July 03, 2017 at 11:50

Hello

Riggs.Rob

,

I will raise your reported issue internally for further investigation and wewill keep you informed about the taken actions/explanation if needed.

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen