STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Problems with CubeMX and MDK-ARM

Posted on June 15, 2017 at 21:54Hi, I'm trying to develop my own libraries to use a lux sensor MAX44009 with an STM32L476RG-Nucleo. I've modified the example I2C_TwoBoards_ComPolling and using its configuration I was able to set up and read the valu...

How can I use audio codec in STM32CubeMX?

Posted on June 06, 2017 at 19:48Hello.I use STM32CubeMX for programming of a STM32F407 Discovery board.I want to play a sound using audio codec.Unfortunately I can't communicate with codec by I2C and I2S.There is no any sound in headphone.Is there a...

Generating code of STM32072B-EVAL from CubeMX

Posted on June 08, 2017 at 10:48Hi,i'm trying to generate code of STM32072B-EVAL via CubeMX, the Tollchain i use is MDK-ARMV5.I notice that the board support in manage run-time environment didn't match with STM32072B-EVAL evaluation board and it rep...

Resolved! STM32F303VB: ADC HAL.. not implemented?

Posted on June 01, 2017 at 13:47Hi,I'm using STM32CubeMX (STM32Cube_FW_F3_V1.8.0) to generate ADC HAL code for my custom board based on STM32F303VB.I see that ADC HAL is not implemented. Only API is givenIs it available in new releases (if any) ?Is ...

Prasant J by Associate III
  • 1079 Views
  • 4 replies
  • 0 kudos

Bug: CDC_Control_FS() in usbd_cdc_if.c is empty

Posted on May 25, 2017 at 22:17I've experienced random and unexplainable problems with CDC communication over USB, while using CubeMX-generated code.The PC was always able to enumerate the COM port, but sometimes it was unable to open it, (Windows r...

0690X00000606zFQAQ.png
infor by Associate III
  • 2225 Views
  • 2 replies
  • 0 kudos

STM32F4 works twice as fast

Posted on May 25, 2017 at 13:10I use SW4STM32. I noticed that when I generate a project with SW4STM32, the speed of my STM32F401VBT6 is twice faster. For example, HAL_Delay(1000) actually awaits 500ms. USART1 transmits data on the speed 230400, alth...

Resolved! Can stm32F446 TIM2 run at 180Mhz

Posted on May 24, 2017 at 11:49Hi, I've got this from the F446 data sheet.I hope that I can run TIM2 at 180MhzHowever, it seems that APB1 peripheral CLK can only run at 90Mhz as the cubeMX indicates as followed:So can I really make TIM2 run at 180MH...

0690X00000602SQQAY.bmp 0690X00000602OjQAI.bmp
Zt Liu by Senior III
  • 2164 Views
  • 4 replies
  • 0 kudos

stm32f4CubeMx IAR ethernet + lwip project, eth receive problem

Posted on October 11, 2016 at 13:52Hi, I'm creating new project for CubeMx and using freeRtos and lwip. i was able to get eth tx workin(verified in tcpdump) dhcp request with correct mac. I was unable to get ethernet to react on receive -> there is...

teijo by Associate II
  • 1638 Views
  • 3 replies
  • 0 kudos