STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1559 Views
  • 0 replies
  • 2 kudos

How to create STM32CubeMX project from an example ?

Hello,On starting a new project with new board, we need to have a STM32CubeMX, but in the cubeH7 example package, I do not find any STM32CubeMX project file.How do I create STM32CubeMX project file with the example ?Thanks,ran

ranran by Senior II
  • 1620 Views
  • 4 replies
  • 0 kudos

Resolved! Does cubeMX have the correct AXI / AHB limits for STM32H750?

Hi,Looking at the block diagram in the datasheet, ABH1, AHB2, AHB3, AHB4, AXI are listed as supporting 200MHz.Cube (v5.0.0, H7 v1.3.0) however will not allow them to be set higher than 100 MHz, and says the must be <- 100MHz in the hover text.Is cube...

JSchl.8 by Associate
  • 1328 Views
  • 1 replies
  • 0 kudos

how to migrate Library Expansion with cubemx5?

hifor example i download https://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-led1.htmlbut cubemx cant add it !problem during load of selected file.this pac...

SChar.8 by Associate II
  • 1606 Views
  • 2 replies
  • 0 kudos

CubeMX Examples, Timers & No .ioc Files?

Hello:I am trying to come to an understanding using timer configurations with CubeMX/HAL. I hope someone can point me in the right direction. This is specifically for timer capture, but is probably applicable to PWM generation, and/or PWM capture too...

Compile with Makefile on Ubuntu 18.04 LTS

Hi,I am trying to compile a generated Makefile project on an Ubuntu machine (18.04 LTS). The compilation works fine on Windows 10.But on Ubuntu, I get the following error:kai@ubuntu:~/workspace/makefile_test$ make arm-none-eabi-gcc build/main.o build...

smrtkai by Senior
  • 3811 Views
  • 4 replies
  • 0 kudos

CubeMX has tiny text on HiDPI screens

All text in the CubeMX standalone application is really small when viewed on a HiDPI screen. Some symbols and controls are also too small.Please make sure that text and symbol size adapts to the screen resolution.