STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1579 Views
  • 0 replies
  • 2 kudos

Hangs in SDIO after update CumeMX

Hello.After updating CubeMX to the latest version, the microSD card is no longer formattedMounting, creating files and writing to them is normal.When calling a function:f_mkfs("", FM_FAT32, 0, work, sizeof work);Hangs up in the HAL_SD_WriteBlocks fun...

RKhal.19 by Associate II
  • 1932 Views
  • 5 replies
  • 0 kudos

Resolved! Can use cubemx to generate lwip project in stm32h743

Posted on June 30, 2018 at 15:49Hi all:     Now I use stm32h743zi, using cubemx to generate LwIP project, but the LwIP option is gray. Dose anyone know that how to fix this. The following picture is the picture what I confige the cubemx project. Tha...

Yi Zhou by Associate III
  • 2571 Views
  • 3 replies
  • 0 kudos

Resolved! Any difference between STM32CUBE_MX And Atollic_TrueStudio?

Right at the moment I have 2 software, Atollic TrueStudio & STM32CUBE_MX . I am pretty confused, which one to use for an STM32-Cortex M4 ? Is there any difference between Atollic TrueStudio & STM32CUBE_MX software? Which one is stable? thanks

vmekr by Associate II
  • 2483 Views
  • 3 replies
  • 0 kudos

STM32CubeMX not running on macOS

After updating the STM32CubeMX Eclipse Plugin to 5.0.0 version I get the following message on running the plugin: "This release of STM32CubeMX Eclipse Plugin cannot be used in macOS".The Plugin still opens, but I can't edit the peripheral values (it'...

flavio23 by Associate III
  • 3427 Views
  • 7 replies
  • 0 kudos

How to enable external interrupt.

I'm using CubeMX V 5.0.1 to create a simple project for Nucleo-L031K6 board. I've configured PA12 as an input. Under Pinout & Configuration->System Core->NVIC there is no option to enable "EXTI line 4 to 15 interrupts" . Show only enabled interrupts ...

STM32CubeMX USB Serial Number String from UID

Posted on March 30, 2018 at 18:03 Hello, I have a device based on STM32F1 series that's using the USB CDC interface. TrueSTUDIO project is generated with STM32CubeMX. Everything is working fine except one last thing: Setting the serial number ...

STM32F746 Disco board - How to enable external SDRAM

Hi,I am new to STM32 systems and CubeMX5 and have several questions.I am using STM32F746 disco board with TrueStudio , I am trying to work with external SDRAM (first time working with external RAM) I configured the FMC and generate the code but all t...

davidra7 by Associate II
  • 4140 Views
  • 8 replies
  • 0 kudos