cancel
Showing results for 
Search instead for 
Did you mean: 

Extremely slow CubeMX in Clock View on OSX.

ChrisH
Associate III
Posted on December 06, 2016 at 21:19

Cube slows down the point when it is pretty much very hard to use. Sometimes clock resolver ends up in an continous loop which leads nowhere. Also on chips with more pins like BGA packages Cube slows down noticeably. Not sure how it is on Windows or Linux as I only use OSX for development.

#stm32cubemx
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Nesrine M_O
Lead II
Posted on December 07, 2016 at 09:20

Hi

Hockuba.Krzyszto.002

‌,

Could you please precise inwhich CUBEMX version you have found the issue. So, we can verify it.

-Nesrine-

Ifmy suggestanswers your question, please mark it as correct.Thank you

root
Associate II
Posted on December 07, 2016 at 11:54

Hello,

Same here on Windows 10, the clock view is very slow, and obviously is doing a lot of (useless) calculations as my laptop starts blowing air while on this page !

Can't remember which version I was running, but I updated to latest version (4.18.0) and still the same !

It used to work very good some months ago, now it is barely usable.

Need a fix ASAP.

Thomas.

Posted on December 07, 2016 at 11:39

Hi

ELMHIRI.Syrine

‌ it's on the new version of CUBE 4.0.

Posted on December 07, 2016 at 11:42

Hi

Hockuba.Krzyszto.002

‌,

I'll report this issue to our MXteam for checking.

Sorry for the inconvenience it may bring.

-Nesrine-

Ifmy suggestanswers your question, please mark it as correct.Thank you

Posted on December 07, 2016 at 12:02

Hi

Legrand.Thomas

‌,

The issue has been reported internally.

Sorry for the inconvenience it may bring.

-Nesrine-

Ifmy suggestanswers your question, please mark it as correct.

Posted on December 07, 2016 at 12:30

Hello,

Just to make sure, I uninstalled STM32CubeMX (including configuration, etc) and reinstalled it.

Same behavior.

Thomas.

Sirma Siang
ST Employee
Posted on February 22, 2017 at 17:09

Hello All,

A high CPU usage when enterring in Clock tab, has bee resolved in 4.19.

Could you please test with this version ?

Thanks in advance.

Kind regards

Sirma

Posted on February 28, 2017 at 14:28

It didn't resolve the issue moreover often 'clock resolver' gets stucked in a loop where there is no way to cancel 'Searching solution' . Which results in losing work if it wasn't saved before this is extremely annoying issue.

Posted on February 28, 2017 at 18:03

Hello,

Could you share the ioc file of theproject on which you face this issue ?

Kind regards

Sirma