cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX generates broken SW4STM32 code

jeremyh
Associate II
Posted on December 31, 2016 at 08:52

Hi,

I've created a very simple project in STM32CubeMX for the F3DISCOVERY board. The only things I changed from the default are enabling MCO, and setting the PLL multiplier to When I import the code into SW4STM32 and press build, I get the following error:

17:41:40 **** Build of configuration Debug for project test_64mhz ****
make all 
Building file: ../Src/main.c
Invoking: MCU GCC Compiler
/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Debug
arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -D__weak=__attribute__((weak)) -D__packed=__attribute__((__packed__)) -DUSE_HAL_DRIVER -DSTM32F303xC -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Inc' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/STM32F3xx_HAL_Driver/Inc' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/STM32F3xx_HAL_Driver/Inc/Legacy' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/CMSIS/Device/ST/STM32F3xx/Include' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/CMSIS/Include' -Os -g3 -Wall -fmessage-length=0 -ffunction-sections -c -fmessage-length=0 -MMD -MP -MF'Src/main.d' -MT'Src/main.o' -o 'Src/main.o' '../Src/main.c'
/bin/sh: -c: line 0: syntax error near unexpected token `('
/bin/sh: -c: line 0: `arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -D__weak=__attribute__((weak)) -D__packed=__attribute__((__packed__)) -DUSE_HAL_DRIVER -DSTM32F303xC -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Inc' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/STM32F3xx_HAL_Driver/Inc' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/STM32F3xx_HAL_Driver/Inc/Legacy' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/CMSIS/Device/ST/STM32F3xx/Include' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/CMSIS/Include' -Os -g3 -Wall -fmessage-length=0 -ffunction-sections -c -fmessage-length=0 -MMD -MP -MF'Src/main.d' -MT'Src/main.o' -o 'Src/main.o' '../Src/main.c''
make: *** [Src/main.o] Error 2
17:41:40 Build Finished (took 94ms)�?�?�?�?�?�?�?�?�?�?�?

My operating system is OSX Yosemite, and both SW4STM32 and STM32CubeMX are updated to the latest versions.

Thanks,

Jeremy

#stm32cubemx #sw4stm32
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Andrei Chichak
Lead II

Posted on December 31, 2016 at 09:00

This has been reported to ST and the people at AC6 that take care of SW4STM

<LINK NO LONGER ACTIVE>

https://community.st.com/0D50X00009Xke6gSAB

Andrei

Nesrine M_O
Lead II

Posted on January 02, 2017 at 11:06

Hi

Herbert.Jeremy

‌,

The issue has been reported to our MXteam for checking.

Sorry for the inconvenience may bring.

-Nesrine-

We are looking for your wishes about our STM32 products,ecosystem and community:

<LINK NO LONGER ACTIVE>

asergeev
Associate II
Posted on January 10, 2017 at 16:21

https://community.st.com/0D70X000006SK0JSAW

 
stm32cube-t
ST Employee
Posted on January 16, 2017 at 13:53

Dear Users,

This issue (encountered on MAC and Linux OS only) will be fixed with STM32CubeMX 4.19 next release.

Best regards

Alain VIEILLARD
Associate
Posted on January 18, 2017 at 17:20

Dear User,

Indeed, this is a regression introduced by Ac6 into the v1.13.

A fix is already under implementation. As temporary solutions, the 2 following workarounds are proposed :

1 – Workaround #1:

In the following post, the user reverted the installation (back to V1.12) and it solved the issue.

http://www.openstm32.org/tiki-view_forum_thread.php?forumId=7&comments_parentId=4390#threadId7

How to revert : Help menu >> Installation Details >> Installation History tab >> Select the V1.12 configuration >> Revert

2 – Workaround #2:

  1. Navigate to <SW4STM32_INSTALL>/plugins/fr.ac6.mcu.externaltools.arm-none.win32/tools/make;

  2. Make a backup of the folder;

  3. Remove the files:

echo.exe

msys-1.0.dll

msys-iconv-2.dll

make/msys-intl-8.dll

msys-regex-1.dll

msys-termcap-0.dll

sh.exe

Sorry for inconveniences.

Best regards,

Alain

Joachim SUSS_O
Associate
Posted on January 18, 2017 at 23:23

Good evening ,

I've a similar issue on my IDE (eclipse), I use STM32CubeMX (the lastet, updrade done 18 January 2017).

During compilation I've this message on eclipse

23:17:50 **** Incremental Build of configuration Debug for project Horloge_CC ****

make all

Building file: ../Src/crc.c

Invoking: MCU GCC Compiler

/home/joachim/workspace/Horloge_CC/Debug

arm-none-eabi-gcc -mcpu=cortex-m7 -mthumb -mfloat-abi=hard -mfpu=fpv5-sp-d16 -D__weak=__attribute__((weak)) -D__packed=__attribute__((__packed__)) -DUSE_HAL_DRIVER -DSTM32F746xx -I'/home/joachim/workspace/Horloge_CC/Inc' -I../Drivers -I../Middlewares -I../Drivers/STM32F7xx_HAL_Driver -I../Middlewares/USB_Device_Library  -O0 -g3 -Wall -fmessage-length=0 -ffunction-sections -c -fmessage-length=0 -MMD -MP -MF'Src/crc.d' -MT'Src/crc.o' -o 'Src/crc.o' '../Src/crc.c'

/bin/sh: 1: Syntax error: '(' unexpected

Src/subdir.mk:66: recipe for target 'Src/crc.o' failed

make: *** [Src/crc.o] Error 2

23:17:50 Build Finished (took 63ms)

I've done a similar project without cube with no problem. I use linux Debian (3.16.0-4-amd64 #1 SMP Debian 3.16.36-1+deb8u2 (2016-10-19) x86_64 GNU/Linux)

Who can help  me ?

Regards

Joachim

Posted on January 18, 2017 at 23:51

select your eclipse project in Project Explorer, then right click

choose 'Properties'

choose C/C++ Build

choose Symbols

change __weak=__attribute__((weak)) to __weak='__attribute__((weak))'

change __packed=__attribute__((__packed__)) to __packed='__attribute__((__packed__))'

Sirma Siang
ST Employee
Posted on January 27, 2017 at 12:25

Hello All,

Eclipse plugins has been patched.

You can check for updates, and upgrade to version 1.13.1.201701200843

Kind regards

Sirma

Posted on February 20, 2017 at 10:56

Hello,

the problem is present again in 'OpenSTM32 IDE 1.13.1.201701261206', running on Windows 10 64bit