STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

Found a bug with the latest rev of STM32CubeMX Rev 5.3.0

I just migrated to CubeMX Rev 5.3.0. I'm developing a project for the Nucleo STM32F429ZI board. My target toolchain is Keil MDK-ARM V5. I'm using mostly the LL function libraries. I'm using the latest FW_F4 V1.24.1 package. Bug: As soon as regenerate...

MSilv by Associate
  • 793 Views
  • 0 replies
  • 0 kudos

SensorTile and CubeMX integration

Hello, I've been learning and using CubeMX a lot for project generation. I work with VS code and compile via make through the generated makefile and it is going pretty good.Now I have to work with the SensorTile and I really wish to use the cube con...

ANist by Associate III
  • 2792 Views
  • 6 replies
  • 0 kudos

Unable to install patch 1.10.1 for STM32F0 offline

I tried to install the en.patch_cubefw_f0.zip package from the "From Local ..." menu in the "Embedded Software Packages Manager" and I receive the message "Missing dependency for this package. - STM32Cube FW_F0 V1.10.0". Unfortunately, the "missing" ...

HAL_TIM_PeriodElapsedCallBack Doesn't works.

Hello,I upgraded cube on version 1.5.3 and function HAL_TIM_PeriodElapsedCallBack stopped working.I found out that program never goes trough function HAL_TIM_PeriodElapsedCallBack .I think that the problem is in initialization , because you need to ...

0690X000009Z8GoQAK.png 0690X000009Z8GjQAK.png 0690X000009Z8GZQA0.png 0690X000009Z8GeQAK.png
NIvez by Associate
  • 1223 Views
  • 0 replies
  • 0 kudos

CubeMX Utility useful update!

Hi! I'm often working with STM32 MCUs and use CubeMX for project creation since it's very useful for such purposes. But what is bothers me the most is that CubeMX generate sections for usercode, where I should write.I understand that it was made for ...

Lenoe by Associate II
  • 1188 Views
  • 1 replies
  • 0 kudos