STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

Resolved! Update Manager has stopped connecting

Hi, I performed a clean re-install of CubeMX and am now having network connectivity problems.Machine: Win10 Home (v1809)CubeMX Version: v5.3.0Install Loc: C:\Sw\stm\STM32CubeBoot Error: Updater Settings:Update Manager:I can browse online and ping goo...

0690X000009YwjDQAS.png 0690X000009YwjIQAS.png 0690X000009YwjNQAS.png
Justin1 by Senior
  • 2415 Views
  • 5 replies
  • 0 kudos

General info on CubeMX generated projects.

I'm using the latest STM32CubeMX Version 5.3.0 (July 2019). I'm trying to wrap my head around the general project structure. Let's take for example a NUCLEO-F767ZI project generated by CubeMX.I'll go through a few conclusions I've drawn so far.1. The...

Change memory map of application using STM32CubeMX

Hello,For a project generated with STM32CubeMX I have to update the memory map in the linker file to be able to use it with a bootloader. The linker file is generated by CubeMX but I don’t see an option to define the starting address of the applicati...

Bug: CMSIS RTOS v2 missing memory pool functions

When CubeMX project is generated with FreeRTOS enabled and using CMSIS RTOS v2, function definitions for memory pool functionality are declared in 'cmsis_rtos2.h' file but their implementations are completely missing from 'cmsis_rtos2.c' or anywhere ...

Error downloading FW.F1.1.7.0 MCU package

Hi,recently I installed STM32CubeMX. When I click 'Check for update' menu item 'STM32CubeF1 Firmware Package V1.7.0 / 09-October-2018' is shown. But when I press 'Install Now' the following error happens:In the log I see:2018-11-20 23:56:39,197 [ER...

Dmitri by Associate II
  • 5998 Views
  • 12 replies
  • 0 kudos

No output on MCO1 after generating code from CubeMx

Hello,I have used CubeMx to generate a project which should do the following:configure PA8 as MCO1 and on it I want to output HSI clock which as I understand is by default 16MhzSo in CubeMx I configured PA8 as MCO1.The generated code was this:/* USER...

0690X000009YwZXQA0.png
PPopo by Senior
  • 2477 Views
  • 6 replies
  • 0 kudos