Skip to main content
Craig B
Associate III
June 8, 2017
Question

STM32CubeMX v4.21 _Error_Handler definition issues in main.h

  • June 8, 2017
  • 10 replies
  • 6122 views

Posted on June 08, 2017 at 02:02

Hi ST,

There are a couple issues with the definition of _Error_Handler() in main.h as generated in v4.21.0. 

First of all it needs to be wrapped as follows so it can be included in both .c and .cpp files with the correct linkage:

#ifdef __cplusplus
extern "C" { 
#endif
 
void _Error_Handler(char *, int); 
 
#ifdef __cplusplus
}
#endif
 
#define Error_Handler() _Error_Handler(__FILE__, __LINE__)

BTW, this should be done for all function definitions in all header files so they work correctly in both .c and .cpp files. I'm sure there are other cases. This is just the one I've run into.

Secondly, the _Error_Handler function is defined as taking a char * for the first argument. However, in gcc __FILE__ is a const char *, so in the macro in the header:

#define Error_Handler() _Error_Handler(__FILE__, __LINE__)

an error is generated. It should be:

void _Error_Handler(const char *, int);

Thanks,

Craig

This topic has been closed for replies.

10 replies

ST Technical Moderator
June 15, 2017
Posted on June 15, 2017 at 14:13

Hi

Broadbooks.Craig

,

I reported this issue internally to our CubeMx team.

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Craig B
Craig BAuthor
Associate III
September 21, 2017
Posted on September 21, 2017 at 02:39

Hi ST team,

I just downloaded and installed the latest CubeMx version for windows and this issue I reported above back in June has not been resolved and a number of releases have happened since.  I know this seems like not a big deal.  However, may I remind you that anyone(including me) who includes main.h in a .cpp module as it is generated with CubeMx has a project that won't build due to the errors in main.h.  That makes this a Class A bug in my book.  If I had a developer on my team who continued to check in or deploy code that didn't build, they wouldn't be around long.  Why is this bug still here?  It means that I have a hand modified main.h that gets overwritten every time CubeMx generates code and I have to revert the necessary changes to it every time.  Not cool!  

Come on guys, you're better than this.

Craig

Efim Ginter
Visitor II
November 22, 2017
Posted on November 22, 2017 at 12:02

the problem is still not solved   

:(

((((
Cyril FENARD
ST Employee
October 25, 2018

Hi all,

ErrorHandler() signature is moving to function with no parameter in the future release.

As far __cplusplus guards are concerned STM32CubeMX has made improvements since several releases.

This issue could be closed.

Regards.

Cyril

PLamo
Visitor II
December 4, 2018

So ST now has made it impossible to output the file and line of the error and this won't be fixed? What's next - generate fully broken code and say it will not be fixed in a future release?

This is broken. Code depends on the file and line of the error. A parameterless error handler is useless. Why would you make an critically important feature useless? No one can upgrade to the newer version of STM32CubeMX.

Tesla DeLorean
Guru
December 4, 2018

>>Why would you make an critically important feature useless? 

Exactly, good grief, who owns the validation and debugging tasks here?

Dumping into an infinite loop with no idea how it got there, how bloody insane is that?

You really can't do this in embedded equipment and expect to keep your job.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PLamo
Visitor II
December 4, 2018

The fix for this is to add your own _Error_Handler() function to main.c and add macros to main.h:

#define GET_MACRO( _0, _1, NAME, ... ) NAME

#define Error_Handler(...) GET_MACRO( _0, ##__VA_ARGS__, Error_Handler1, Error_Handler0 )()

#define Error_Handler0() _Error_Handler( __FILE__, __LINE__ )

#define Error_Handler1(unused) _Error_Handler( char * file, int line )

void _Error_Handler(char *, int);