STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1708 Views
  • 0 replies
  • 2 kudos

Resolved! Problem installing on Mac Best Answer

Downloaded and installed the latest Java development kit. Tried installing SetupSTM32CubeMX-6.0.1 via: sudo java -jar SetupSTM32CubeMX-6.0.1.exe but get this error message: Error: Unable to access jarfile SetupSTM32CubeMX-6.0.1.exe .Any ideas?

0693W000003PPG6QAO.png
MBudz.1 by Associate II
  • 5059 Views
  • 12 replies
  • 0 kudos

Resolved! Create ioc from project files??

I'm using STM32CubeMX V6.0.1. I have a project for which there is not a CubeMX ioc file for. I do know the project was created using CubeMX. Is there a way to re-generate the ioc from the project files??ThanksTom

tweb by Associate
  • 1565 Views
  • 2 replies
  • 0 kudos

CubeMX does not handle IO alternate functions and peripherals

Hello,I have a project where I use a L010K8 (LQFP32 package).Let say that you want to keep PA13 and PA14 for SWD debugging and use PA15 as USART2 Tx.Now PA15 AF4 is USART2 Rx, but this can be swapped in USARTx->CR2.First point is that Rx/Tx swap is n...

Kraal by Lead
  • 2489 Views
  • 5 replies
  • 0 kudos

Resolved! STM32CubeMX generates wrong RAM size for STM32H745BITx

When using STM32CubeMX v6.0.1 to generate a project for dual-core STM32H745BIT6 MCU the resulting linker files for CM4 and CM7 show the following memory structures:CM7MEMORY { FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K RAM (xrw) : ORI...

0693W000003QWiTQAW.png
davhak by Associate II
  • 1664 Views
  • 1 replies
  • 0 kudos

Resolved! I2C between two stm32 board

I am working on a project which needs data communication between two stm32 (f103rb and f429zg). I use stm32f103rb-nucleo examples_ll (I2C _OneBoard_Communication_IT) but it works for one byte and after that it stops working. I want it to work repetit...

darestani by Associate II
  • 1806 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.