STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

STM32CubeIDE does not retain user code in FreeRTOS tasks when regenerating with Project Manager Generated Files change

In STM32CubeIDE V1.4.2, if the CubeMX Project Manager has the "Generate peripheral initialization as a pair of '.c/.h' files per peripheral" setting enabled after the project had been built with it previously disabled, when the project code is re-gen...

dlkeng by Associate III
  • 2051 Views
  • 3 replies
  • 0 kudos

About using STM32F072CBT6 as USB Peripheral device

Hello guys , I am using the stm32f072 microcontroller as a usb peripheral device to use it as Serial Device . I have programmed it successfully and it works fine almost time but sometime it crashes the usb interface of my system. I have tried it on o...

KJangu.2 by Associate II
  • 1970 Views
  • 3 replies
  • 0 kudos

TCP ECHO CLIENT/SERVER IN NUCLEO-F207ZG

Hello everyone, I've brought a new NUCLEO-F207ZG for some development purpose. and it is working really fine. And thanks to ST support I've found so many good sample code with STM32CubeMX ( en.stm32cubef2 ) . As one of my important task is to im...

Resolved! STM32CubeMX bug for Save Project

I disable “DMA1 stream0 global interrupt�?,and then click Fiel-》save project ,then close STM32CubeMX。But when I open the project next time, “DMA1 stream0 global interrupt�? is still enabled。I do not know why? hwo can help me,think you�?

0693W000004IBAsQAO.png
lshao.1 by Associate
  • 1362 Views
  • 3 replies
  • 1 kudos

STM32CubeMX 6.0.1 released

What is new in STM32CubeMX V6.0.1? Minor release fixing the issues reported belowFixed issues 90615 Unexpected project data deletion when some utilities are used. 90636 IRQ priorities for some "Non-System" IPs are set to minimal values after project ...

Help with HRTIM UPDATE GATING

I have the problem, that the following code does not update the registers.// The update events, as mentioned below, can be: MSTU, TFU, TEU, TDU, TCU, TBU, TAU, TxRSTU,TxREPU LL_HRTIM_TIM_SetUpdateGating(HRTIM1, LL_HRTIM_TIMER_E, LL_HRTIM_UPDATEGATING...

MHeid.1 by Associate
  • 1349 Views
  • 1 replies
  • 0 kudos

Resolved! Using STM32CubeMX 6.0.1 with STM32429I-EVAL board. Want to configure FreeRTOS (CMSIS_v2 API) with MPU support - but MPU is greyed out...

But there's an example project behind the scenes showing how to enable MPU (STM32CubeF4\Projects\STM324x9I_EVAL\Applications\FreeRTOS\FreeRTOS_MPU).I would really like to use STM32CubeMx to configure the project - but it looks to me like its not poss...

Torben1 by Associate II
  • 1305 Views
  • 1 replies
  • 0 kudos