2020-03-27 3:28 AM
I have added the library but I cannot build the project because there is a call to TP_STM32_MotionFX_Library_Init in StartDefaultTask (I am using FreeRTOS and Atollic) that appears to be missing from the library.
If I comment out this line, the call to MotionFX_initialize does not return.
I cannot send the entire source as this is a commercial project, but I can send pieces if required.