STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1722 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMX Generate wrong code for I2S Master-Transmit, or F302 has bug? (CubeMX ver 1.4.2 + STM32Cube_FW_F3_V1.11.1 + STM32F302R8)

Dear Experts,I ported I2S RX and TX program from F401 to F302R8 Nucleo board. And I encountered **unexpected** phenomenon.When I use I2S for receiving data (Half-duplex, Master-Receive mode, 48kHz, 24bit data on 32bit frame), it works fine. That mean...

KAJIK.1 by Associate III
  • 1679 Views
  • 2 replies
  • 0 kudos

CubeMX doesn't allow Fadc > 18 MHz for H743 Rev. V

If from the "Clock Configuration" tab Fadc > 36Mhz then the Clock prescaler for the ADC is automatically set to /2 where the /1 is diabled. For > 72MHz it is /4 where /1 and /2 are disabled. Rev. 2 has an additional /2 divider that has been taken int...

Wde G.1 by Associate II
  • 1175 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.