STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1628 Views
  • 0 replies
  • 2 kudos

Resolved! How to configure FileX using CubeMX?

How to start with FileX using CubeMX?In CubeMX I enabled ThreadX and FileX with the default configuration, increased ThreadX "memory pool size" to 2k and  enabled "Generate Init Code" for both.In app_azure_rtos.c, tx_application_define() function MX_...

STM32-ThreadX-1.png STM32-ThreadX-2.png
TDJ by Lead
  • 8491 Views
  • 11 replies
  • 4 kudos

Resolved! Cannot configure MbedTLS in CubeMX for H755

When trying to setup MBedTLS through CubeMX for the NUCLEO-H755ZI-Q, CubeMX does not give the option to select LWIP as the TCP/IP stack in the MBEDTLS "Version and modes" configuration tab. The only options given are "None" and "User defined". Additi...

SPetr.6 by Associate III
  • 1663 Views
  • 5 replies
  • 0 kudos

Resolved! loading code from external flash on STM32N6570-DK

I have just purchased the STM32N6570-DK kit and have been able to successfully load and run the demo binaries. However when I have tried to generate a simple application like the LED Blink project I have been able to successfully get it running in th...

digilog by Associate II
  • 735 Views
  • 1 replies
  • 0 kudos

Resolved! NETXDUO lan8742 added twice to Makefile

Dear community,we're using a Makefile Project with STM32H5xx and NetX Duo using the LAN8742When the code is generated, CubeMX is adding the line:.../STM32Cube/Repository/STM32Cube_FW_H5_V1.1.1/Drivers/BSP/Components/lan8742/lan8742.c \twice to the Ma...

stst9180 by Associate III
  • 4696 Views
  • 8 replies
  • 2 kudos

problems with making generate code

When I create a new GPIO port configured as OUTPUT in STM32CubeMX, the pin definitely exists on my board. However, after I click Generate Code, the new pin configuration does not appear in main.c (for example, I don’t see the initialization code for ...

tal333 by Associate
  • 684 Views
  • 2 replies
  • 2 kudos

Resolved! STM32CubeMX CAD Export Options (e.g. KiCAD) missing

Hello ST Community,STM32CubeMX 6.16.0 release summary:– Migrated to SamacSys as a new CAD provider for STM32CubeMXWith the new version of the stm32cubemx, the CAD tab in tools (see screenshot) is missing the previously available KiCAD and other optio...

M_Schmidt_0-1764079018385.png M_Schmidt_1-1764080134218.png
M_Schmidt by Associate III
  • 819 Views
  • 3 replies
  • 6 kudos