Skip to main content
Associate II
February 6, 2024
Question

CubeMX bug regarding LPUART1 DMA (MX_Device.h)

  • February 6, 2024
  • 3 replies
  • 1216 views

I use the STM32L496ZG. When generating the files using STM32CubeMX it also generates MX_Device.h which contains several defines. When using LPUART1 with DMA it also generates defines like:

#define MX_LPUART_RX_DMA_DMA_Handle
#define MX_LPUART_RX_DMA_Instance DMA2_Channel7

The CMSIS Driver for the UART however uses:

#ifdef MX_LPUART1_RX_DMA_Instance
 #define UART6_DMA_USE_RX UART_DMA_USE_RX
#else
 #define UART6_DMA_USE_RX 0
#endif

So using MX_LPUART1_RX_DMA_Instance is not the same as MX_LPUART_RX_DMA_Instance and causes the DMA to be disabled.

MX_Device.h should contain LPUART1 instead of LPUART with regards to the DMA defines as it also does with the Pin and IRQ defines.

This topic has been closed for replies.

3 replies

ST Technical Moderator
February 6, 2024

Hello @Reneb  ,

First let me thank you for posting and welcome to the ST Community.

Your request is under investigation, and I will get back to you ASAP.

For more investigation I suggest also that you provide your ioc file.

Thanks.

Mahmoud.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
RenebAuthor
Associate II
February 6, 2024

Hello @Mahmoud Ben Romdhane,

Attached you'll find the ioc file.

Regards,