STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 2 kudos

Resolved! Issue when upgrading FreeRTOS plugin

Hi!I have an issue with the upgrade process of the X-CUBE-FREERTOS plugin. It happened upgrading to 1.3.0 and to 1.3.1 as well: the list of tasks defined in CubeMX seems to be retained in the CMSIS RTOS2 tab as well as the other settings, but when re...

paolog by Senior
  • 2130 Views
  • 9 replies
  • 3 kudos

STM32N6 FDCAN Baudrate not changed

Hi, I’m working with the STM32N6 board and need to configure the FDCAN1 parameters. I’m using the 64 MHz internal clock, and I calculated the bit rate using the Bit Rate Calculator. I want to set a baud rate of 500 kbps, but I’m unable to do so. The ...

STM32 CubeMx Exception

Hi,I am running into thread exception while running CubeMx on MacOs M4 Pro.Platform: MacOs M4 ProCubeMx (About):  Java (21.0.8 (9))  [STM32CubeMX 6.16.0 Mac ARM]When I try to open Airoc-Wi-Fi-Bluetooth Pack under Middleware, I get following exception...

JenishR_0-1763423820908.png
JenishR by Associate
  • 572 Views
  • 3 replies
  • 1 kudos

Resolved! We found a bug while using Hardware JPEG.

The environment I tested is as follows.​IDE: STM32CubeIDE​ 1.5.1Package: STM32F767IIPackage software version: 1.16.1​JPEG settings are as below.​​However, there is a typo in the config file that is actually generated.[ jpeg_utils_conf.h ]#ifndef __J...

0693W00000Czw4kQAB.png

Resolved! STM32H755 model switch from LQFP to BGA In CubeMx

Hi, I have been using NUCLEO-H755ZI_Q board for initial software development and evaluation. I wanted to use STM32H755IIK3 but as nucleo version was not available, I have been working with LQFP144 version. I want to switch MCU model to this BGA and m...

mosamasa by Associate II
  • 705 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CubeIDE doesn't save clock configuration

Hi, I'm facing a problem with the Clock Configuration tab with the latest version of the STM32CubeIDE. In fact, every time I open the ioc file, there is an error with the SMPS Clock Mux on the STM32WB board I'm using. I correct and generate code and ...