STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1626 Views
  • 0 replies
  • 2 kudos

Resolved! STMCubeIDE problem with repository directory

Hi,With CubeMX I can adjust where the repositories are saved. This function is missing in CubeIDE and its also not using the same from CubeMX.Because the saved files are huge, then I get problem when I login/logout in the company. Because the files a...

Osto by Senior
  • 2966 Views
  • 2 replies
  • 0 kudos

STM32L433 - LPUART1 wrong baudrate

Hello,I'm using STM32L433RCT-P nucleo board and I was testing some hardware. I noticed the baudrate error with LPUART1 is really high (135100 instead of 115200, 67570 instead of 57600).I have no problem using manual configuration instead of CubeMX, ...

MFran.4 by Senior
  • 1165 Views
  • 1 replies
  • 0 kudos

STM32CubeMX won't finish generating code and is stuck.

Hi.I am working with a STM32F030x8 microcontroller.I am using KEIL uVision5 version 6.2.0 to test some C code on the microcontroller.From what I understand, I need to generate a startup file in order to build the code properly.Without it I get: ERROR...

0693W00000ANVEZQA5.png
PSchj.1 by Associate
  • 1761 Views
  • 2 replies
  • 0 kudos

Resolved! Why is CubeMX trying to enable Overclocking in my project?

I created a new project for an STM32F407VE and when the code is generated CubeMX puts this in SystemClock_Config: /** Activate the Over-Drive mode */ if (HAL_PWREx_EnableOverDrive() != HAL_OK) {  Error_Handler(); }When you try to compile it, it gets ...

MStra.3 by Associate III
  • 1707 Views
  • 2 replies
  • 0 kudos

OSX version do not respond to mouse click

latest Catalina and cube mx fresh install. And I can only click on pins to select function but no clicking of left side list items makes me unable to set HSE resonator. What is wrong?

hijax_pl by Associate III
  • 2035 Views
  • 5 replies
  • 0 kudos

Resolved! STM32H745I-DISCO, problem porting QSPI_MemoryMappedDual example on a brand new CubeMX project with default initialization of the board.

Started with the example that can be found on STM32H7 Github at https://github.com/STMicroelectronics/STM32CubeH7/tree/v1.9.0/Projects/STM32H745I-DISCO/Examples/QSPI/QSPI_MemoryMappedDual , I tried to port it into a brand new project generated with C...

one shot mode

Configuration: 1. timer2 configured as one shot mode2. PA0 acts as IC1,and TI1FP1;PA1 acts an OC2.3.connect external trigger(3.3V LVTTL) to the TI1FP14. cubemx followedQuestion:1.Before enable CCER->CC1E, the amplitude high is 3.3V. While execute the...

Jtee.1 by Associate II
  • 1460 Views
  • 2 replies
  • 0 kudos