STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1592 Views
  • 0 replies
  • 2 kudos

I would like to know tried and tested way to interface STM32F469 SPI port to a 3 wire Synchronous serial interface device. Also want to know how to use STMCubeMX/IDE to configure the SPI port to talk to the device and what programming effort may be need

Using STM32F469 DISO and STM32F469VGT6 LQFP package for our board. The device to be interfaced with STM32F469 SPI port has the following pin outs Serial data input/output pin1 Serial data input pin2 Serial interface clock pin Chip select

PRama.3 by Associate II
  • 1208 Views
  • 1 replies
  • 0 kudos

STMH743ZI2 CubeMx clock setup, max frequency not allowed

I have been following this discussion: https://community.st.com/s/question/0D50X0000AIclNC/nucleoh743zi-stm32h7-400mhz-stm32cubemx-will-not-configure-to-400mhzAs when I create a project for the Nucleo-H743ZI2 I have to set the clock, and the auto gen...

0693W000008z6mjQAA.png
KSOdin2 by Associate III
  • 2828 Views
  • 1 replies
  • 0 kudos

Resolved! How to enable output compare timer interrupt in STM32CubeMX?

Hello,I want to activate three output compare interrupts in my timer peripheral. I want to use Output Compare for this purpose because then I can change the time. However, in STM32CubeMx there is a button to activate a global TIM2 interrupt, but ther...

0693W00000APxORQA1.png 0693W00000APxP0QAL.png
Eden.757 by Associate
  • 5830 Views
  • 1 replies
  • 0 kudos