STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1711 Views
  • 0 replies
  • 2 kudos

Resolved! STM32H SAI setting for 8-PDM microphones

I would like to know how we can configure STM32H7's SAI(s) for 8-PDM microphone inputs (LR * 4 pairs). (16kHz sampling rate).It seems MX allows us 6 mic with SAI1 and 2 mics with SAI4 but I'm not sure how we can set SAI1/4 exactliy for 8 mics (synchr...

YKiku.2 by Associate
  • 2525 Views
  • 1 replies
  • 0 kudos

I am creating a codes from STM32CubeMx. Every code generated from the CubeMx (6.2.1) is going in hard fault when I open in CubeIde (Ver 1.6.1). I could not understand where is the problem?

Request cumunity member to guide on this topic. I am unable to download any single code which is generated from the CubeMx for Cubeide. Each generated code is going in hard fault.Please tell me the issue and suggest correct way if I am doing any mist...

DSaha.3 by Associate II
  • 5681 Views
  • 12 replies
  • 0 kudos

STM32F407G RTC & SD Card(SPI) Not working simultaneously

Hello,I am developing a board based on STM32F407G (Disc1) Where I am connecting an SD-Card over the SPI to store some data in the file on SD card. I am configuring internal RTC for the time tracking, On internal clock, a 16x2 LCD connected via 4-bit ...

DParm.1 by Associate II
  • 2798 Views
  • 4 replies
  • 0 kudos

Heap_x.c file not in GPDSC file generated by STM32CubeMX

Hi, I've generated a project using STM32CubeMX for the STM32G030C8Tx and I've included FREERTOS. The heap_x file is not listed in the GPDSC file. I think this is a bug, note someone else appears to have had the same issue here: Topic: Error undefined...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.